×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 35438898, Entry date: 08/10/2009
(0)
Rate

Micro Memory Card (MMC) also as SIPLUS version?

  • Entry
  • Associated product(s)
QUESTION:   Are the SIMATIC Micro Memory Cards (6ES79*) also available as SIPLUS versions (6AG19*)? ...

QUESTION:  

Are the SIMATIC Micro Memory Cards (6ES79*) also available as SIPLUS versions (6AG19*)?

ANSWER:

The SIMATIC Micro Memory Card is not available as SIPLUS version. Tests have shown that the SIMATIC Micro Memory Cards can be used in SIPLUS modules for a temperature range of -40°C...+70°C and under medial loads/bedewing.

Information about SIPLUS products is available at http://www.siemens.com/siplus

If you have further questions, please get in touch with your SIMATIC partner in your Siemens subsidiary

Siemens Partners in the Internet


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.