×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 35533333, Entry date: 05/28/2009
(1)
Rate

SINAMICS Support Packages (SSP) SINAMICS S110 V4.1, SINAMICS V2.6.1 and SINAMICS G120 V3.2.0.0

  • Entry
  • Associated product(s)

DESCRIPTION:

Support for SINAMICS S110 V4.1.0.0, SINAMICS V2.6.1.0 and SINAMICS G120 V3.2.0.0 with SIMOTION SCOUT V4.1 SP2 HF4

The appropriate SINAMICS Support Packages (SSPs) can already be downloaded here as support for SINAMICS S110 V4.1.0.0, SINAMICS V2.6.1.0 and SINAMICS G120 V3.2.0.0 versions.

It is sufficient to load the STARTER_V41SP2HF4_VOL_3.zip filed that is saved there.

The missing SSPs can also be installed in the particular SSP directory in SIMOTION SCOUT V4.1 SP2 HF4 using setup.exe.

SINAMICS S110:
SSP_SINAMICS_S110_04_10_16_00_04_07_00_00.zip ( 42919 KB )

SINAMICS S120:
SSP_SINAMICS_02_60_35_00_04_03_00_00.zip ( 268962 KB )

SINAMCIS G120:
SSP_SINAMICS_G120_03_20_28_00_04_00_00_00.zip ( 16115 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.