×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 35955048, Entry date: 11/17/2009
(1)
Rate

CEMAT V7.0 Service Pack 1 for SIMATIC PCS 7 V7.1

  • Entry
  • Associated product(s)

CEMAT V7.0 + Service Pack 1 (SP1) has been released for operation with SIMATIC PCS 7 V7.1. Please note that SIMATIC PCS 7 V7.1 must always be installed before CEMAT V7.0 + SP1. Beyond that no further restrictions exist. However, when converting existing or creating new CEMAT projects please always read the information on how to update the SIMATIC PCS 7 software from V6.x or V7.0 to V7.1 as described in the user manual "SIMATIC PCS 7 V7.1 - Software updating without using new functions". Addendum dated Nov. 09, 2009: The WinCC User Archive License required for SIMATIC PCS 7 V7.1 is now also included in the software package S79220-B1834-P (CEMAT V7.0 SP1)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.