×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 36489314, Entry date: 01/09/2012
(1)
Rate

Which panels are certified for the FM explosion protection standard for North America?

  • Entry
  • Associated product(s)

Product information
This entry contains all the SIMATIC HMI panels that have an FM certificate for the explosion protection standard. The FM certification is valid exclusively for North America.

Note
In Europe, the explosion protection guidelines in compliance withATEX are valid. More information on the panels that Siemens currently provides with ATEX certification is available in Entry ID: 291285.

Contents

  1. Information on FM certification
  2. Current HMI panels with FM certificate
  3. Discontinued HMI panels with FM certificate
  4. Explanation of terms

Pay attention to the explosion protection ID on the back of the device before installing the panels. Panels mentioned in the certificate should not be used automatically in the hazardous areas with potentially explosive atmosphere. What counts here is the ID on the back of the device.

1. Information on FM certification
The classification of the explosion protection in the NEC (National Electric Code) is standard in the United States of America and that in the CEC (Canadian Electric Code) in Canada.

The hazardous areas/divisions with potentially explosive atmosphere are defined in the NEC 500. In addition, in the NEC 505, the hazardous areas with potentially explosive atmosphere are divided into zones in the same way as in ATEX and have practically identical types of protection. The specifications in the NEC 500 regulate conventional Ex classification (Class Division Model) and include the classification of the new zone model that is based on regulations in Europe and the IEC. Based on this, testing organizations like FM (and FMRC - Factory Mutual Research Corporation) create their own sets of standards.

2. Current HMI panels with FM certificate
The following panels have been tested in compliance with the FM certification NI Class I, Division 2, Group ABCD and Class I, Zone 2, Group IIC.

Note
Details about FM certification are available in the relevant certificates.

The panels in the following table are sold by Siemens (as at 05/2009).
 

Key Panels MLFB Certificate
KP8 6AV3688-3AY36-0AX0 15247146
KP8F 6AV3688-3AF37-0AX0 15247146
Micro Panels MLFB Certificate
TD200 6ES7 272-0AA30-a
6ES7 272-0AA31-a
19182993
TD200C 6ES7 272-1AA10-a 19182993
TD400C 6AV6 640-0AA00-0AX1 29567488
TP177micro 6AV6 640-0CA11-a 22554901
15247146
Operator Panels MLFB Certificate
OP77A 6AV6 641-0BA11-a 24535989
15247146
OP77B 6AV6 641-0CA01-a 15247146
OP177B DP 6AV6 642-0DC01-a
OP177B PN/DP 6AV6 642-0DA01-a
Touch Panels MLFB Certificate
TP177A 6AV6 642-0AA11-a 22554901
15247146
TP177B DP 6AV6 642-0BC01-a 15247146
TP177B PN/DP 6AV6 642-0BA01-a
TP177B PN/DP (OEM) 6AV6 642-7BA11-a
TP177B 4" Color Panel PN/DP 6AV6 642-0BD01-a 15247146
TP177B INOX color 6AV6 642-8BA1a-a
TP277 6" 6AV6 643-0AA01-a
Comfort Panels MLFB Certificate
KTP400 Comfort 6AV2124-2DC01-0AX0 15247146
KP400 Comfort 6AV2124-1DC01-0AX0 15247146
TP700 Comfort 6AV2124-0GC01-0AX0 15247146
KP700 Comfort 6AV2124-1GC01-0AX0 15247146
TP900 Comfort 6AV2124-0JC01-0AX0 15247146
KP900 Comfort 6AV2124-1JC01-0AX0 15247146
TP1200 Comfort 6AV2124-0MC01-0AX0 15247146
KP1200 Comfort 6AV2124-1MC01-0AX0 15247146
Multi Panels MLFB Certificate
MP177 6" 6AV6 642-0EA01-a 15247146
MP277 8" Touch 6AV6 643-0CB01-a 15247146
MP277 10" Key 6AV6 643-0DD01-a
MP277 10" Touch 6AV6 643-0CD01-a
MP277 INOX 10" Touch 6AV6 643-8AD10-a
MP277 INOX 10" Touch Ex 6AV6 643-0ED01-a
MP377 12" Key 6AV6 644-0BA01-a 15247146
MP377 12" Touch 6AV6 644-0AA01-a
MP377 INOX 15" Touch 6AV6 644-0CB01-a
MP377 15" Touch 6AV6 644-0AB01-a
MP377 19" Touch 6AV6 644-0AC01-a
a

-

includes all alphanumerical order numbers.

3. Discontinued HMI panels with FM certificate
The following panels have been tested in compliance with the FM certification NI Class I, Division 2, Group ABCD and Class I, Zone 2, Group IIC.

Note
Details about FM certification are available in the relevant certificates.

The panels in the following table are discontinued and cannot be ordered any more.
 

Text Displays (COROS) MLFB

Certificate

OP3 6AV3-503-1DB10-a

16668227

OP5 A1
OP5 A2
6AV3-505-1FBa-a
OP15 A1
OP15 A1-VF
OP15 A2
OP15 A2-VF
6AV3-515-1EBa-a
OP15 C1
OP15 C2
6AV3-515-1MAa-a
Graphics displays (COROS) MLFB Certificate
OP25 6AV3-525-1AEa-a

16668227

OP35 mono 6AV3-535-1FAa-a
OP35 color 6AV3-535-1TAa-a
Micro Panels MLFB Certificate
TP170micro 6AV6 640-0CA01-a 15247146
TP070 6AV6 545-0AA15-a
Operator Panels MLFB Certificate
OP170B Mono 6AV6 542-0BB15-a 15247146
OP270 6" Key 6AV6 542-0CA10-a
OP270 10" Key 6AV6 542-0CC10-a
Touch Panels MLFB Certificate
TP170A 6AV6 545-0BA15-a 15247146
TP170B Mono 6AV6 545-0BB15-a
TP170B Color 6AV6 545-0BC15-a
TP170B INOX 6AV6 545-8BC10-a
TP270 6" Touch 6AV6 545-0CA10-a 15247146
TP270 10" Touch 6AV6 545-0CC10-a
TP270 10" Touch INOX 6AV6 545-8CC10-a
Multi Panels MLFB Certificate
MP277 6" Touch 6AV6 545-0AH10-a 15247146
MP270B 10" Key 6AV6542-0AG10-a
MP270B 10" Touch 6AV6 545-0AG10-a
MP370 12" Key 6AV6 542-0DA10-a 15247146
MP370 12" Touch 6AV6 545-0DA10-a
MP370 15" Touch 6AV6 545-0DB10-a
MP370 Touch INOX 6AV6 545-8DB10-a
C7 devices MLFB Certificate
C7-636 Touch 6ES7 636-2EBa-a 29567757
MOBIC MLFB Certificate
MOBIC T8 6GK1611-0TA01-a 17166214
a

-

includes all alphanumerical order numbers.

4. Explanation of terms
In the following, we briefly explain only the relevant designations.

  • Nonincendive (NI)
    This type of protection is provided specially for Division 2 and specifies that during normal operation no sparks and no hot surface temperatures are generated. The type of protection is comparable with the type of protection "n" in compliance with EN 50021.
     
  • Class I, Division 2 (NEC 500)
    Areas where dangerous concentrations of flammable gases or vapors do not exist under normal operating conditions.
     
  • Class I, Zone 2 (NEC 505)
    Areas where dangerous concentrations of flammable gases or vapors do not exist under normal operating conditions.
     
  • Group A, B, C, D (NEC 500)
    The division into "Groups" refers to the hazardous materials:

    A = Air/gas mixture with acetylene
    B = Air/gas mixture with hydrogen
    C = Air/gas mixture with ethylene
    D = Air/gas mixture with propane
     
  • Group IIC (NEC 505)
    The division of the "Group" (NEC 505) is equivalent to the explosion group in the ATEX guidelines. Hydrogen is defined as a typical gas in explosion group IIC.
     
  • Temperature classes T*
    There are six different temperature classes that are specified in detail in compliance with NEC 500-3. The temperature class includes the highest permitted surface temperature of the apparatus and provides information on the ignition temperatures of the inflammable materials.

Keywords
Ex protection, USA

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.