×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 36645252, Entry date: 06/17/2013
(20)
Rate

How can you reset WinCC flexible to the original status of the last installation?

  • Entry
  • Associated product(s)

Introduction
In some cases, it might be necessary to reset WinCC flexible to the status immediately after installation. For example, it might happen that various windows (Tools windows, for example) are no longer displayed properly. If this behavior occurs, one option is to delete the cache of WinCC flexible.

Description
Proceed as follows to delete the cache of WinCC flexible.

WinCC flexible 2004/ WinCC flexible 2005/ WinCC flexible 2007
WinCC flexible 2008

WinCC flexible 2004/ WinCC flexible 2005/ WinCC flexible 2007
You reset the WinCC Flexible ES as follows for the versions WinCC flexible 2004, WinCC flexible 2005 and WinCC flexible 2007.

  1. Close WinCC flexible.
  2. Terminate the running processes "Hmies.exe" and "HmiSmartStart.exe" in the "TaskManager".
  3. If the following directories exist, delete the entire contents (alternatively you can also back up the contents).

    C:\Documents and Settings\All Users\Application Data\SIEMENS AG\SIMATIC WinCC flexible 2007
    C:\Documents and Settings\USER NAME\Application Data\SIEMENS AG\SIMATIC WinCC flexible 2007
    C:\Documents and Settings\USER NAME\Local Settings\Application Data\SIEMENS AG\SIMATIC WinCC flexible 2007
     
  4. Start WinCC flexible 2007 and create a new project.

Notes
The path might be different if you have installed WinCC flexible or the operating system on a different partition.
When you delete the contents of the "Temp" folder, there might be problems, for instance, if files are being accessed at the time. Delete as many files as possible.
After a reset, the startup of WinCC flexible takes a little longer, because the ES has to be reinitialized completely.
You can also use the "Hmies.exe -reset -new" command to reset the versions WinCC flexible 2005 and WinCC flexible 2007.

WinCC flexible 2008
As from the version WinCC flexible 2008 you have the "Reset SIMATIC WinCC flexible" option in the "SIMATIC WinCC flexible Start Center". This resets WinCC flexible to the original status of the last installation.
 

No. Procedure
1 Select the option in the "SIMATIC WinCC flexible Start Center":
Right-click the "Start Center". Now the menu is displayed. Select the option "Reset SIMATIC WinCC flexible".


Fig. 01

Note
Upon installation, an icon is created in the taskbar Notification Area, the so-called Tray Area, for operating the "WinCC flexible Start Center".

2 Confirm security prompt
Confirm the security prompt with "OK" to reset WinCC flexible 2008.


Fig. 02

Now the cache of WinCC flexible is cleared. Upon termination, the program starts automatically with the Start page.

Note
If the "Reset SIMATIC WinCC flexible" option is grayed out, proceed as follows.
 

No. Procedure
1 Close WinCC flexible and STEP 7.
2 Start the Windows Task Manager close all the processes with HmiES.exe.
3 Restart your computer.

Note
If the "Reset SIMATIC WinCC flexible" option is not in the taskbar, proceed as follows.
 

No. Procedure
1 Check whether the "SIMATIC WinCC flexible Start Center" symbol for the taskbar is hidden.
  • Click the arrow next to the input language selection.


Fig. 03

  • Check whether the "SIMATIC WinCC flexible Start Center" symbol for the taskbar is hidden.


Fig. 04

  • You can display the "SIMATIC WinCC flexible Start Center" symbol by means of "Customize..." > In the event display "Display symbols and messages".
2 Check whether the "SIMATIC WinCC flexible Start Center" is in the Auto Start.
  • Click "Start".
  • Enter "msconfig" in the Search Bar.
  • In the "System Configuration" window that opens you click the "Startup" tab.
  • Add WinCC flexible and/or enable it.


Fig. 05

Information on the topic of "Adding a program to the Windows Autostart" is available here.

3 Start the "SIMATIC WinCC flexible Start Center" with "C:\Programs\Siemens\SIMATIC WinCC flexible\WinCC flexible 2008\ HmiSmartStart.exe".
Or click "Start" and enter "HmiSmartStart.exe" in the Search Bar.

Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.