×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 36727563, Entry date: 01/30/2018
(5)
Rate

Which SIMATIC HMI operator panels and Industry PCs have a shipbuilding certificate?

  • Entry
  • Associated product(s)
Shipbuilding certificates of the classification societies for SIMATIC HMI operator panels and Industry PCs

Before installing a SIMATIC HMI panel or Industry PC you should note whether the device is listed in the certificate and whether type-specific changes have to be made. Without this change the device does not have a certificate for shipbuilding.

1. Information about the shipbuilding certificate

The classification societies are responsible for classifying ships. A ship must be classified before it can sail for the merchant navy and before it can be insured along with its cargo. SIMATIC HMI Panels are certified by the following classification societies:
 

AbbreviationClassification societyCountry
ABSAmerican Bureau of ShippingUSA
BVBureau VeritasFrance
DNVDet Norske VeritasNorway
GLGermanische LloydGermany
LRSLIoyd's Register of ShippingGreat Britain
NKNippon Kaiji KyokaiJapan
PRSPolski Rejestr StatkówPoland
RINARegistro Italiano NavaleItaly
RMRSRussian Maritime Register of ShippingRussia
CCSChina Classification SocietyChina
 KRKorean Register of ShippingKorea

Note
New certificates are DNV-GL certificates. A distinction is made between DNV and GL notified bodies.

2. Current HMI panels with shipbuilding certificate

A precise search for certificates available for HMI operator panels is available at the following link in our Online Support Portal:

SIMATIC HMI operator panels with a shipbuilding certificate

You can further refine this search by selecting the approval office and/or country.


Fig. 01

Select "All Products" to find out which devices are included in the certificate.

Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.

3. Current Industry PCs with shipbuilding certificate

A precise search for certificates available for Industry PCs is available at the following link in our Online Support Portal:

SIMATIC Industry PCs with a shipbuilding certificate

You can further refine this search by selecting the approval office and/or country.


Fig. 02

Select "All Products" to find out which devices are included in the certificate.

 
Additional Keywords
Classification, Shipbuilding certificate
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit