Entry type: FAQ, Entry ID: 36727563, Entry date: 04/16/2015
(2)
Rate

Which panels are certified for shipbuilding?

  • Entry
  • Associated product(s)
This entry contains all the SIMATIC HMI panels that have a certificate for shipbuilding from the classification societies.

Before installing the panel, note whether the panel is listed in the certificate and whether type-specific changes have to be made. Without such changes the panel does not have a shipbuilding certificate.

1. Information about the shipbuilding certificate

The classification societies are responsible for classifying ships. A ship must be classified before it can sail for the merchant navy and before it can be insured along with its cargo. SIMATIC HMI Panels are certified by the following classification societies.
 

Code Classification society Country
ABS American Bureau of Shipping USA
BV Bureau Veritas France
DNV Det Norske Veritas Norway
GL Germanische Lloyd Germany
LRS LIoyd's Register of Shipping Great Britain
NK Nippon Kaiji Kyokai Japan
PRS Polski Rejestr Statków Poland
RINA Registro Italiano Navale Italy
RMRS Russian Maritime Register of Shipping Russia
CCS China Classification Society China

 

2. Current HMI panels with shipbuilding certificate

The following panels have been certified by various shipbuilding classification societies.

Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.

The panels in the table below are currently sold by Siemens.
 

Basic Panels MLFB Link
KTP400 Basic mono 6AV6647-0AA11-3AX0 available certificates
KTP400 Basic color PN 6AV6647-0AK11-3AX0 available certificates
KTP600 Basic mono PN 6AV6647-0AB11-3AX0 available certificates
KTP600 Basic color DP 6AV6647-0AC11-3AX0 available certificates
KTP600 Basic color PN 6AV6647-0AD11-3AX0 available certificates
KTP1000 Basic color DP 6AV6647-0AE11-3AX0 available certificates
KTP1000 Basic color PN 6AV6647-0AF11-3AX0 available certificates
KTP1500 Basic color PN 6AV6647-0AG11-3AX0 available certificates
Comfort Panels MLFB Link
KP400 Comfort 6AV2124-1DC01-0AX0 available certificates
KTP400 Comfort 6AV2124-2DC01-0AX0 available certificates
KP700 Comfort 6AV2124-1GC01-0AX0 available certificates
TP700 Comfort 6AV2124-0GC01-0AX0 available certificates
KP900 Comfort 6AV2124-1JC01-0AX0 available certificates
TP900 Comfort 6AV2124-0JC01-0AX0 available certificates
KP1200 Comfort 6AV2124-1MC01-0AX0 available certificates
TP1200 Comfort 6AV2124-0MC01-0AX0 available certificates
Micro Panels MLFB Code
OP73micro

6AV6640-0B..

available certificates
TP177micro

6AV6640-0CA1..

available certificates
Operator Panel MLFB Code
OP73 6AV6641-0A..
available certificates
OP77A 6AV6641-0B..
available certificates
OP77B 6AV6641-0C..
available certificates
OP177B DP 6AV6642-0DC01-1AX0
available certificates
OP177B PN/DP 6AV6642-0DA01-1AX0
available certificates
OP277 6" 6AV6643-0B..
available certificates
Touch Panels MLFB Code
TP177A 6AV6642-0A..
available certificates
TP177B 4" 6AV6642-0BD01-3AX0
available certificates
TP177B DP 6AV6642-0BC01-1AX..
available certificates
TP177B PN/DP 6AV6642-0BA01-1AX0
available certificates
TP277 6" 6AV6643-0A..
available certificates
Multi Panels MLFB

Code

MP177 6" 6AV6642-0EA01-3AX..
available certificates
MP277 8" Key 6AV6643-0DB01-1AX..
available certificates
MP277 8" Touch 6AV6643-0CB01-1AX..
available certificates
MP277 10" Key 6AV6643-0DD01-1AX..
available certificates
MP277 10" Touch 6AV6643-0CD01-1AX..
available certificates
MP377 15" Touch Daylight 6AV6644-8AB20-0AA1 available certificates
1) Certificates in preparation.

 Additional Keywords
Classification, Shipbuilding certificate