Entry type: FAQ, Entry ID: 36752540, Entry date: 02/23/2015
(1)
Rate

Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) with topological configuration and device replacement without topological configuration?

  • Entry
  • Associated product(s)

Description

Automatic commissioning (device replacement without interchangeable medium) with topological configuration
IO devices which support automatic commissioning (device replacement without interchangeable medium) can be easily replaced.
These IO devices are distinguished by the following properties:

  • There is no need for an interchangeable medium (Micro Memory Card, for example) with saved device name.
  • The device name does not have to be assigned to the PG.

The replacement IO device receives the device name from the IO controller and not from the interchangeable medium or the PG. For this the IO controller uses the configured topology and the neighbor relationships determined by the IO devices. Here, all the participating devices must support the LLDP (Link Layer Discovery Protocol). The configured nominal topology must match the actual topology.

The IO controllers below support automatic commissioning (device replacement without interchangeable medium):

36752540_PROFINET_IO_Controller_list_en.pdf ( 64 KB )

The IO devices below support automatic commissioning (device replacement without interchangeable medium):

36752540_PROFINET_IO_Device_list_en.pdf ( 67 KB )

Device replacement without topological configuration

ET 200SP
If the device name is saved in addition on the bus adapter (BA 2xRJ45 or 2xFC) of the interface module, you can replace it without PG and without topological configuration.
By saving on the bus adapter and on the interface module you have different scenarios when using the device name.
 

  Interface module empty Interface module with device name
Bus adapter empty No device name available. Device name from interface module is used and copied to bus adapter.
Bus adapter with device name Device name from bus adapter is used and copied to interface module. Device name from the bus adapter is used and copied to the interface module if this has a different device name.

With the interface module below the device name is stored in addition on the bus adapter:

  • ET 200SP IM 155-6 PN HF with article number 6ES7155-6AU00-0CN0 firmware V2.0 and higher
  • ET 200SP IM 155-6 PN ST with article number 6ES7155-6AA00-0BN0 and 6ES7155-6AU00-0BN0 firmware V3.1 and higher

ET 200pro
The interface module IM154-4 PN High Feature and the connection modules CM IM PN M12, 7/8" and CM IM PN PP Cu all have an internal memory in which the device name is stored. Therefore there are different scenarios for the validity of the device name when replacing a module without PG.
 

Device name scenarios Device name validity
Device name in CM and IM = empty MAC address (no device name)
Device name in CM=IM or IM=CM Device name CM
Device name in CM≠IM or IM≠CM Device name CM
Device name in CM=ok and in IM=empty Device name CM
Device name in IM=ok and in CM=empty Device name IM

With the interface module below the device name is stored in addition on the connection module:

  • ET 200pro IM 154-4 PN with article number 6ES7154-4AB10-0AB0 firmware V6.0 and higher

 

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster