Entry type: FAQ, Entry ID: 36955473, Entry date: 06/03/2014
(0)
Rate

Evaluation of a safety function by using SIMATIC S7 "standard output cards" switched off by the load voltage

  • Entry
  • Associated product(s)

QUESTION:

How to evaluate a safety function by using SIMATIC S7 "standard output cards" switched off by the load voltage?

 

 

ANSWER:

ISO 13849-1
IEC 62061

Explanation for the application:

Following explanations attempt the possible evaluation of SIMATIC S7 standard output cards with IEC 62061 or ISO 13849-1.

The statements below do not contain any claim to completeness but should be a practical support in the comprehension and implementation of IEC 62061 or ISO 13849-1.

Attached you find a document which explains this issue detailed.


Anymore questions?
Please consult Siemens - Technical Assistance for Industrial Controls via mail address or phone number, as shown in the header of the attached document.

IEC62061_ISO13849_Info_5_en.pdf ( 42 KB )