×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 36969886, Entry date: 09/08/2009
(1)
Rate

Printing of WinCC flexible/ Audit

  • Entry
  • Associated product(s)

Task:
An MP 277 shall be used for controlling a “bread baking plant”. Using this example plant it should be possible to trace all operator actions at a later point in time as well. Setting the temperature at the oven shall only be allowed for certain users. A protocol shall be printed out via a printer.

Solution:
The panel is used with the option WinCC flexible/Audit.
The application shows how an Audit Trail can be stopped safely, printed and restarted. The MP 277 was used as operating device.

The following figure displays the most important components of the solution.

Downloads

Content of the downloads

Download

Documentation (English) 36969886_WinCC_flexible_Audit_en.pdf ( 944 KB )
Code 
WinCC flexible 2008 project (WinCC flexible 2008 SP1)
WinCC_flexible_Audit.zip ( 2765 KB )

 

History

Issue

Modifications

09/2009 First issue

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.