Entry type:
FAQ
Entry ID:
37208360,
Entry date:
06/08/2015
Rate
Which virus scanner versions can you use for STEP 7 V5.3 to V5.7?
-
Entry
-
Associated product(s)
Information on compatibility with virus scanners can be found in this entry and in the Compatibility Tool.
Description
The following table contains the virus scanners that have been tested for compatibility with the specified STEP 7 version. You can operate this virus scanner in the standard setting.
STEP 7 version | Virus scanner |
---|---|
V5.7 |
|
V5.6 |
|
V5.5 |
|
V5.4 |
|
V5.3 |
|
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations. The Compatibility Tool contains the following information:
- New compatibility information
- New tool functions
- Tool operating instructions and help
Compatibility information for STEP 7 V5.4 and higher is available in the Compatibility Tool. Further information is available under the entry ID: 64847781.
Additional Keywords
compatibility, virus scanner
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
- French
- Italian
- Spanish
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC Software for SIMATIC Controller STEP 7 V5.x STEP7 basic software and editors STEP 7
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC Software for SIMATIC Controller STEP 7 V5.x STEP7 basic software and editors STEP 7 Professional
Rate entry
Requests and feedback
What do you want to do?
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information
Topic pages for this entry