×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 37361207, Entry date: 07/10/2009
(2)
Rate

Smith Predictor for Control of Processes with Dead Times

  • Entry
  • Associated product(s)

Objective of the Application
The objective is fast and tight control of processes with dead times. A dead time can be recognized by the observation that after a step excitation of the manipulated variable there is no reaction of the controlled variable at all for a certain time (the dead time). A normal PI controller must be tuned very sluggish for processes with large dead times and the control performance will decrease accordingly. The control performance can be considerably improved with the help of a so-called Smith-Predictor.

The present example shows the realization of a control loop with PI controller and Smith-Predictor starting from the respective process tag type (CFC solution template) of the PCS 7 Advanced Process Library.

Main contents
The following main points are discussed in this application note:

  • How to create an instance and set the parameters of the process tag type.
  • How to calculate the required process model for the Smith-Predictor.
  • Benchmark simulations with and without Smith-Predictor, to show the potential benefits.

Validity
… valid for PCS 7 V7.1, in principal transferable to V7.0.

Downloads

Content of the downloads

Download

Smith Predictor for Control of Processes with Dead Times 37361207_Smith_Prediktor_en.pdf ( 856 KB )

History

Version

Modification

07/2009 V1.0 First release

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.