Tipo di articolo: Download, ID articolo: 37453235, Data articolo: 11/12/2014
(0)
Valuta

To project a legal-for-trade display for SIWAREX FTA with WinCC flexible a SecureOCX software is provided.

  • Articolo
  • Riguarda prodotto/i

To project a legal-for-trade display for SIWAREX FTA with WinCC flexible a SecureOCX software is provided. Here you find the adequate Software for the different WinCC flexible versions. The HMI panels, which are supporting the SecureOCX software, are listed into the chapter 8.6 of the Siwarex FTA manual. The list of supported HMI panels and the  installation instruction for the legal-for-trade display in WinCC flexible 2008 SP3 are found in the download file OXC_FOR_SECURE_DISPLAY_WinCC_2008_SP3.zip

For use with TIA-Portal the Software SecureDisplay is provided. This can be found at the following Link:
http://support.automation.siemens.com/WW/view/en/107196401  

The Siwarex FTA manual can be downloaded by logging on to:
http://support.automation.siemens.com/WW/view/en/17970155

Please note also the following FAQ:
http://support.automation.siemens.com/WW/view/en/35364527

IMPORTANT NOTE:
If the scale was checked and sealed of a notified body, it is not allowed to change the WinCC flexible software version, e.g. with a software version-update from „WinCC flexible 2008“ to „WinCC flexible 2008 SP1“.
If the WinCC flexible software version will nevertheless changed and a project will downloaded to the HMI panel, the SecureOCX display will work no longer and the error message “ERROR 3” occurs on the SecureOCX display.

Title of the Download
 OCX_FOR_SECURE_DISPLAY_WinCC_2008_SP1.zip ( 386 KB )  
 OCX_FOR_SECURE_DISPLAY_WinCC_2008.zip ( 552 KB )  
 OCX_FOR_SECURE_DISPLAY_WinCC_2007.zip ( 497 KB )
 OCX_FOR_SECURE_DISPLAY_WinCC_2005.zip ( 400 KB )  
 OCX_FOR_SECURE_DISPLAY_WinCC_2008_SP2.zip ( 657 KB )

  OCX_FOR_SECURE_DISPLAY_WinCC_2008_SP3.zip ( 546 KB )

Dettagli errore
Descrizione dettagliata del guasto
Aiutateci a migliorare il Supporto online.
La pagina richiamata non può essere visualizzata. Contattare il webmaster.
Contattare il webmaster