×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 37885119, Entry date: 08/07/2009
(1)
Rate

Displaying values of the SENTRON PAC3200 / PAC4200 in WinCC 7.0 SP1 via Ethernet

  • Entry
  • Associated product(s)

QUESTION:

How can WinCC 7.0 SP1 display values of SENTRON PAC3200/PAC4200 via Ethernet?



ANSWER:

Measured values of SENTRON PAC3200 and PAC4200 can be transmitted via Ethernet with Modbus TCP/IP Driver and displayed in WinCC 7.0 SP1.

 

The attached file shows you further details.


68375_76.pdf ( 177 KB )


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.