×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 37939948, Entry date: 08/29/2013
(0)
Rate

What support does Siemens AG offer to make products comply with FDA regulations?

  • Entry
  • Associated product(s)

Food & Drug Administration (FDA)


FDA logo

The FDA is the USA authority for licensing drugs and is under the Ministry of Health. The FDA was founded in 1927 with headquarters in Rockville (Maryland).

The FDA's task is to protect public health in the USA. It regulates the safety and effectiveness of human and animal pharmaceuticals, biological products, medical products, food and radiating devices. The regulations apply to products produced in the USA and imported products.
The FDA is comparable with the TÜV and Ministry of Health in Germany.

Important regulation for Siemens AG products
On August 20, 1997, the FDA's rule 21 CFR Part 11 on electronic records and signatures came into force. 21 CFR Part 11 (in brief: Part 11) defines the acceptance criteria of the FDA for the use of electronic records and signatures instead of drawings in paper form and handwritten signatures on paper.

The requirements include the following:

  • Validation
  • Records of operator actions
  • Retention/Protection/Reproducibility/Retrievability
  • Access protection
  • Electronic signature (certification of equality)

Detailed information on the single products and solutions are available at the following links.
 

Description Entry ID
Information about WinCC. 37940022
Information about WinCC flexible, WinCC flexible Runtime and panels that can be configured with WinCC flexible. 37939984
Information about WinCC (TIA Portal), WinCC Runtime Advanced and panels that can be configured with WinCC (TIA Portal).  37940461
Table 01

Further information about GMP
More information on the topic of GMP (Good Manufacturing Practice) is available at the following link:
http://www.automation.siemens.com/pharma

Additional Keywords
Certificate, Directives, Laws

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit