×
Siemens Industry Online Support
Siemens AG
Type de contribution : FAQ ID de la contribution : 38112017, Date de la contribution : 04/04/2016
(0)
Évaluer

SIMOVERT P (6SE20/21), MICROMASTER, SINAMICS G120 (CU2x0x): Successsor, replacement inverter.

  • Contribution
  • Concerne le/les produits(s)
This FAQ applies only to the SIMOVERT P (6SE20/21), MICROMASTER, SINAMICS G120 (CU2x0x) inverters. Description.

Where can I find a replacement for my old SIMOVERT P, MICROMASTER or SINAMICS G120 (CU2x0x) inverter?

Description
If you want to replace an old inverter with an equivalent one you can use the "DT-Configurator" tool with following link www.siemens.com/dt-configurator .
It is also possible to select an equivalent inverter by using the SIEMENS SIZER tool; Entry-ID: 54992004

For this methode you only need some characteristical data of the old inverter. It is possible to get this data with the PMD Tool (only Siemens internal) or with the following listed characteristical data. As an example the order number 6SE3114-0DC40:


Data Example
Order number   6SE3114-0DC40 6SE6440-2UD21-5AA1
Infeed Line data 3AC 400V / 50Hz 3AC 400V / 50Hz
Interference suppression No No
Energy recovery No No
Inverter Design Chassis Chassis
Power rating 1.5kW 1.5kW
Overload capability 150% / 60s 150% / 60s
Degree of protection IP21 IP20
Control mode V/f V/f
Communication modules Terminal Terminal
Output frequency range 50Hz 50Hz
Motor protection (I²/t, PTC, KTY) I²/t I²/t
Functions (Safety-function, PID-controler, free function blocks) No No
Options Line reactor / output choke No No
Filter No No
Brake resistor No No
Evaluation motor encoder No No
Motor   Asynchronous, 3AC 400V / 50Hz, 1,5kW Asynchronous, 3AC 400V / 50Hz, 1,5kW

Further information
Today's MICROMASTER 4 as well as SINAMICS G120 (CU2x0x) can, in most cases, be replaced by SINAMICS G120 (CU2x0-2).
SINAMICS G120 (CU2x0-2) onwards are compatible from a functional perspective; however they are not compatible from a spare part perspective – i.e. the parameterization must be appropriately adapted.
See therefore:

  • FAQ: What do I have to observe when migrating from a SINAMICS G120 (CU2x0x) or a MICROMASTER 4 to a SINAMICS G120 (CU2x0-2)?; Entry-ID: 64913783
  • FAQ: What must I observe if I wish to replace a SIMATIC ET200S FC converter by a converter from the SINAMICS family?; Entry-ID: 58349882
  • FAQ: What do I have to observe, if I want to replace a CU240D of the SINAMICS G120D with a CU2..D-2? What advantages do I have by making this changeover?; Entry-ID: 60162672
  • FAQ: What do I have to observe if I wish to replace a Control Unit CU240E or CU240S by a Control Unit CU240B-2, CU240E-2 or CU250S-2?; Entry-ID: 70021820
  • FAQ: What do I have to observe if I wish to replace a MICROMASTER MM440 by a SINAMICS G120 with a control unit from the 2nd generation (Firmware ≥ V4.6)?; Entry-ID: 82169413
  • FAQ: What are the differences in the representation of the actual state of the MICROMASTER 4 and SINAMICS G120/G120D frequency inverters after Power on and ON/OFF1 command?; Entry-ID: 28518735

Generally, older inverters have an integrated, basic (simple) operator panel. This is no longer the case for newer inverter types. Operator panels and additional accessories can be found in the “Configurator” under the “Accessories” tab.

Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport