×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 38391227, 文档发布日期 2016年12月12日
(9)
评估

SINAMICS V: Positioning of a V60 using S7-1200 (TIA-Portal) with puls/direction interface and HMI (Set 7)

  • 文档
  • 涉及产品
SINAMICS V60 and CPU1214C with puls/direction interface.

Task
A servo motor is to be moved with a servo drive by Siemens SINAMICS V60 and using the pulse interface of a S7-1200 CPU1214C.

Solution
For the startup we offer you a software example with test code and documentation for controlling the servo drive by the SIMATIC S7-1200.
Both the servo drive and the S7-1200 CPU have an individual internal pulse counter each, whose count represents the current position. Before moving to an absolute position, the counter of the S7-1200 CPU has to be synchronized with the physical position of the axis.
Operation and visualization takes place via a KTP1500 or KTP600 touch panel which is to be connected via an Ethernet connection to the S7-1200 controller.

The task consists of the following scenarios

  • moving the motor in jog mode
  • referencing
  • absolute and relative positioning
  • moving the motor with Command Table (move profiles)


Figure 01

Downloads
  Documentation.pdf (1,5 MB)

 Registrierung notwendig  Project for SINAMICS V60 with TIA V11.zip (2,5 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V12.zip (3,0 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V13.zip (4,6 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V14.zip (1,1 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V15.zip (1,1 MB)

Further Information
What additions are included in the firmware changes of the S7-1200 controllers? 92047260
SINAMCS V60 manual 44254092


Last Changes
Addition the project for SINAMICS V60 with TIA Portal V15. 

Additional Keywords
motioncontrol_apc_applications, PTO, pulse train out, direction


安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.