×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 38391227, Entry date: 12/12/2016
(10)
Rate

SINAMICS V: Positioning of a V60 using S7-1200 (TIA-Portal) with puls/direction interface and HMI (Set 7)

  • Entry
  • Associated product(s)
SINAMICS V60 and CPU1214C with puls/direction interface.

Task
A servo motor is to be moved with a servo drive by Siemens SINAMICS V60 and using the pulse interface of a S7-1200 CPU1214C.

Solution
For the startup we offer you a software example with test code and documentation for controlling the servo drive by the SIMATIC S7-1200.
Both the servo drive and the S7-1200 CPU have an individual internal pulse counter each, whose count represents the current position. Before moving to an absolute position, the counter of the S7-1200 CPU has to be synchronized with the physical position of the axis.
Operation and visualization takes place via a KTP1500 or KTP600 touch panel which is to be connected via an Ethernet connection to the S7-1200 controller.

The task consists of the following scenarios

  • moving the motor in jog mode
  • referencing
  • absolute and relative positioning
  • moving the motor with Command Table (move profiles)


Figure 01

Downloads
  Documentation.pdf (1,5 MB)

 Registrierung notwendig  Project for SINAMICS V60 with TIA V11.zip (2,5 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V12.zip (3,0 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V13.zip (4,6 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V14.zip (1,1 MB)
 Registrierung notwendig  Project for SINAMICS V60 with TIA V15.zip (1,1 MB)

Further Information
What additions are included in the firmware changes of the S7-1200 controllers? 92047260
SINAMCS V60 manual 44254092


Last Changes
Addition the project for SINAMICS V60 with TIA Portal V15. 

Additional Keywords
motioncontrol_apc_applications, PTO, pulse train out, direction


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.