×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 38494882, Entry date: 07/03/2013
(0)
Rate

SIMATIC & SIMOTION: Configuring RT communication between SIMATIC and SIMOTION (I-Device)

  • Entry
  • Associated product(s)

Problem
The I-Device functionality has been available since SIMOTION V4.1.1 in order to exchange data between SIMATIC and a SIMOTION control via PROFINET. This means that in this case the SIMOTION controller acts as "intelligent IO device" = IDevice. This means that data is exchanged between the controls via the I/O areas.
The SIMATIC CPU is the higher-level IO controller in the PROFINET IO system. The SIMOTION control is configured as I-Device and is therefore an IO device of the SIMATIC CPU.
Communication can be established in both directions (bidirectional) via I/O areas using the I-Device functionality.
Further, this function allows both controls to operate in separate projects.
Further, using the I-Device, a machine module can be encapsulated, so that this can then be used several times in a large plant or system.

Solution
In this application, a description is given on how a SIMOTION I-Device connected to a SIMATIC CPU can be configured in order to exchange data between both controls via PROFINET RT.
In the project example, 254 bytes are sent from the SIMOTION control to the SIMATIC CPU. The SIMATIC control then returns the received data, mirrored.

 

 Downloads

Content of downloads

Download

Documentation 38494882_RT_I-Device_V1_4_en.pdf ( 735 KB )
Code
project example, ST units and an address list
 

Security Notice
Caution
The functions and solutions described in this article confine themselves to the realization of the automation task predominantly. Please take into account furthermore that corresponding protective measures have to be taken up in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the Internet. Further information can be found under the Entry-ID 50203404.

Last Changes
V1.3, 06/2012, Revised edition

Additional Keywords
motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.