Entry type: FAQ, Entry ID: 38525996, Entry date: 09/16/2009
(0)
Rate

How can you select messages in WinCC Alarm Control?

  • Entry
  • Associated product(s)

Description:
The new WinCC Alarm Control provides you with the extensive option of selecting messages in Alarm Control during configuration and at Runtime. A detailed description is available in the WinCC Information System in the path: Working with WinCC > Setting up a Message System > Display of Messages during Runtime > Operation during Runtime > How to select messages.

Note:
If you enter a selection with several criteria, these criteria are linked as in an "AND" operation. You can link multiple selections as in an "OR" operation. You can create these selections both during configuration and during Runtime.

Example:
If you enter the criteria "Number less than 100" and "Number greater than 1000" in a selection, no messages are displayed, because this creates the SQL statement "MSGNR < 100 and MSGNR > 1000".

If you create a selection with the criteria "Number less than 100" and a selection with the criteria "Number greater than 1000" and you link these two selections, you get a display of all the messages numbered 1 to 99 and all the messages with numbers greater than 1000. The SQL statement created would be "MSGNR < 100 or MSGNR> 1000".

Instructions for creating selections during configuration:
 

No. Procedure
1 Add a WinCC Alarm Control (not WinCC Alarm Control (Classic) in the Graphics Designer. Open the Properties dialog of the WinCC Alarm Control and select the "Message lists" tab. Select "Selections > Edit...".


Fig. 01

2 Select "New..." to create your desired selection criteria.
3 No messages are displayed with this setting.


Fig. 02

4 With this setting, all the messages numbered 1 to 99 and all the messages with a number greater than 1000 are displayed.


Fig. 03


Fig. 04


Fig. 05

With these settings and links, all the messages numbered 1 to 99 and all the messages with a number greater than 1000 are displayed.

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster