Tipo di articolo: Comunicazione prodotto, ID articolo: 38572895, Data articolo: 25/09/2009
(0)
Valuta

SIMATIC Field PG M2 with pre-loaded STEP 7 Basic V10.5 SP1 Software

  • Articolo
  • Riguarda prodotto/i

Updated SIMATIC pre-loaded software

Effective October 1, 2009, the Field PG M2 can be ordered with updated SIMATIC software.

Field PG M2 "STANDARD" with SXGA+ Display

All Field PG M2 ordered after October 1, 2009 will be equipped with SXGA+ displays, irrespective of whether you order the hardware configurations STANDARD or PREMIUM.

Updated SIMATIC pre-loaded software

All orders for the Field PG M2 received as from October 1, 2009 will be shipped with SIMATIC software as at "09/2009"; the last digit of the order no. changes from "3" to "4".

The following SIMATIC software products will be included in the new pre-loaded software for the Field PG M2, as at "09/2009":

  • SIMATIC STEP 7 Professional 2006 SR6
    (comprises STEP 7 V5.4 incl. SP5, S7-GRAPH V5.3 incl. SP6, S7-SCL V5.3 incl. SP5, S7-PLCSIM V5.4 incl. SP3)
  • SIMATIC WinCC flexible Advanced 2008 SP1
  • SIMATIC STEP 7-Mirco/Win V4.0 incl. SP7
  • SIMATIC STEP 5 V7.23 HF2
  • New: STEP 7 Basic V10.5 SP1

For more details on STEP 7 Basic V10.5 please see SIMATIC Update with entry ID: 38118444

Field PG M2 STANDARD with SXGA+ Display

Effective October 1, 2009, the Field PG M2 with "Standard" configuration will also be equipped with SXGA+ displays.

 

Overview of accessories for the Field PG M2

The scope of supply includes:

  • Software package "Software for Field PG M2"
    • comprising SIMATIC SW and application software on CD/DVD
    • optionally ordered SIMATIC software licenses on 3.5" diskette (no diskette included with TRIAL !)
  • Recovery data carrier for operating system
  • Field PG backpack
  • Wide-range power supply with power cable as ordered
  • Adapter from 25 to 9-pole COM interface
  • Li-Ion battery
  • Modem adapter set
  • Set of documentation

Additional accessories (X) depend on the selected SIMATIC software licenses:

Selected SIMATIC software license MPI Cable S5 PLC Cable S5 EPROM Adapter SMC Card Reader
Trial License for STEP 7 Professional , WinCC flexible Adv.       X
Upgrade STEP 7 Professional, STEP5, WinCC flexible Adv. X     X
Powerpack: STEP 7 Professional
Upgrade: STEP5, WinCC flexible Adv.
X     X
STEP 7 Professional, STEP 5, WinCC flexible Adv. X X X X
STEP 7, WinCC flexible Adv. X     X
STEP 7 Professional, WinCC flexible Adv. X     X

Software Update Service (SUS) for SIMATIC Software

You can purchase a Software Update Service agreement for each of the individual SIMATIC software licenses (STEP 7, STEP 7 Professional, WinCC flexible Advanced). The Software Update Service is not part of the scope of supply of the pre-installed software of the Field PG M2 and must be ordered separately.

Order No. Designation
6ES7810-5CC04-0YE2 SIMATIC S7, STEP 7 Professional Software Update Service for 1 year with automatic renewal, latest software version must be installed
6ES7810-4BC01-0YX2 SIMATIC S7, STEP 7 Software Update Service for 1 year with automatic renewal, latest software version must be installed
6ES7822-0AA00-0YL0 SIMATIC S7, STEP 7 Basic Software Update Service for 1 year with automatic renewal, latest software version must be installed
6AV6613-0AA00-0AL0 WinCC flexible Advanced Software Update Service for 1 year with automatic renewal, latest software version must be installed

Optional accessories for Field PG M2

Order No. Designation
6ES7648-2AG40-0HA0 1 GB DDR2 RAM memory submodule for Field PG M2
6ES7648-2AG50-0HA0 2 GB DDR2 memory submodule for Field PG M2
6ES7798-0GA00-0XA0 External power supply for Field PG M2 / Field PG M
6ES7798-0DA00-0XA0 Field PG backpack
6ES7798-0AA05-0XA0 Li-Ion battery 6.6 Ah Field PG
6ES7900-5AA00-0XA0 Power cable for Field PG for G, F, NL, E, B, A, S, SF
6ES7900-5BA00-0XA0 Power cable for Field PG for Great Britain
6ES7900-5CA00-0XA0 Power cable for Field PG for Switzerland
6ES7900-5DA00-0XA0 Power cable for Field PG for USA
6ES7900-5EA00-0XA0 Power cable for Field PG for Italy
6ES7900-5FA00-0XA0 Power cable for Field PG for China
6ES7790-0AA01-0XA0 USB mouse
6ES7901-0BF00-0AA0 SIMATIC S7 MPI cable, 5m
6ES5734-2BF00 S5 PLC cable 5m
6ES7798-0CA00-0XA0 S5 EPROM adapter
6ES7790-1AA00-0AA0 Serial ATA to USB adapter (only) for Field PG M2 and Field PG M
6ES7791-2BA00-0AA0 Swappable hard disk kit with protective bag and Torx screwdriver
6ES7790-2AA00-0AA0 SMC Reader (Express Card; only for use with Field PG M2!)
A5E00510007 36-month Service Option for SIMATIC Field PG M/M2

Extended Hardware Service for SIMATIC PC / PG products

When you purchase and register for this extended hardware service for a SIMATIC PC / PG, the period of free repairs for the device will be extended to 36 months from the date of delivery.

Scope of services for this option within the period of validity (36 months):

  • Free1) repair during the period of validity at one of our authorized Repair Centers in your vicinity.
    You will find the addresses of our worldwide partners in the Internet under www.siemens.com/asis
  • During the period of validity of the agreement Siemens will bear the costs of the work arising at the Repair Center (labor and materials / spare parts) required for restoration of the operability2) of the hardware.
  • Siemens will furthermore bear the costs of the return transport of the repaired unit from the Repair Center to the customer.

1) This service excludes wear and tear parts as well as problems created by improper handling of the unit.

2) In the case of hard disk defects requiring restoration of the system, only the resoration of the original ex-factory installation is included in the repair service. Uploading of additional user application software, drivers and setting up of the Operating Software is not included in the free repair service.

Ordering and registration of the supplementary agreement:

  • Order the "36-month Service Option for SIMATIC Field PG M/M2" using the above order no.
     
  • Scope of supply:
    Description of services in 4 languages + Service Device Label with License No. to mark the supplementary agreement on the unit.
     
  • Enabling of the Service License No. for a SIMATIC PC / SIMATIC PG via Internet http://www.siemens.com/ped
    The registration must take place within the first 90 days after initial delivery of the unit!