×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 38701812, Entry date: 01/13/2010
(2)
Rate

SIMOTION, SINAMICS S120: Safety Integrated Extended Functions - Failsafe drives on SIMOTION D435 with PROFIsafe control via PROFIBUS slave-to-slave communication

  • Entry
  • Associated product(s)

Task:
A system equipped with SINAMICS S120 drives is controlled by a SIMOTION D435. Various safety functions must be used within the system.
The SIMOTION does not comprise any safety functions. It uses the extended safety functions integrated in the SINAMICS S120 drives.
These drive-integrated safety functions shall be controlled by the F-CPU using the PROFIsafe telegram via PROFIBUS slave-to-slave communication. The safety signals acquired via a failsafe digital input module are processed by the F-CPU and transferred to the drives using the above-mentioned telegram. In this case, the SIMOTION serves as the PROFIBUS master and the F-CPU as I slave. The PROFIdrive communication is established between the SIMOTION and the SINAMICS, the PROFIsafe telegrams are exchanged between the F-CPU and the SINAMICS via the PROFIBUS slave-to-slave communication.

This functional example is based on the SIMOTION D435 training case (6ZB2 470-0AE00), the SINAMICS training case (6ZB2 480-0BA00) and the SAFETY training case.

Solution:
See the following documentation:

Downloads

Download contents

Download

Documentation 38701812_mc_fe_i_011_v10_en.pdf ( 4970 KB )
Project MC_FE_I_011_V10_EN.zip ( 2154 KB )

 History

Edition

Changes

11/2009 First edition

Search term:
motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.