×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 38823708, Entry date: 11/10/2009
(0)
Rate

Product Information: SIMATIC powerrate V3.0

  • Entry
  • Associated product(s)

Starting 10/01/2009, changes with regard to the licensing and the delivery scope will become effective for SIMATIC powerrate:

  • Runtime licenses for the operation on one automation system (AS) will be dropped   
     
  • SIMATIC powerrate Engineering/Upgrade will include the libraries for SENTRON PAC3200 and SENTRON 3WL/3VL



Until 09/30/2009, the licensing model depicted in fig. 1 applies to SIMATIC powerrate:  

Fig. 1

  • Engineering License 
    Permits the operation on one OS* and one AS**
    When using more than one OS, each additional OS requires one Engineering license 
     
  • Runtime License 
    Permits the operation on one additional AS 

*  OS: Operator Station (PCS 7 / WinCC Single-User Station, Server)
** AS: Automation System (S7-CPU)

SIMATIC powerrate License Types (until 09/30/2009)
  WinCC PCS 7
Trial License (for 30 days) 3ZS2795-1CC30-0YG7 3ZS2785-1CC30-0YG7
Engineering + 1 AS Runtime License 3ZS2795-1CC30-0YG0 3ZS2785-1CC30-0YG0
1 AS Runtime License 3ZS2795-1CC30-6YH0 3ZS2785-1CC30-6YH0
Unlimited Runtime License 3ZS2795-1CC30-6YD0 3ZS2785-1CC30-6YD0
Upgrade V2.0 -> V3.0
Engineering + 1 AS Runtime License 
3ZS2795-1CC30-0YE0 3ZS2785-1CC30-0YE0
Upgrade V2.0 -> V3.0
1 AS Runtime License
3ZS2795-1CC30-6YF0 3ZS2785-1CC30-6YF0


Starting 10/01/2009, the Runtime licenses for the operation on one AS will be dropped (paper license): 

  • The Engineering license permits the operation on one operator station (OS) and any number of automation systems (AS). When using more than one OS, each additional OS requires one Engineering license.
SIMATIC powerrate Packages (from 10/01/2009)
  WinCC PCS 7
Trial License (for 30 days) 3ZS2795-1CC30-0YG7 3ZS2785-1CC30-0YG7
Engineering + AS Runtime (unlimited) 3ZS2795-1CC30-0YG0 3ZS2785-1CC30-0YG0
Upgrade V2.0 -> V3.0
Engineering + AS Runtime (unlimited)
3ZS2795-1CC30-0YE0 3ZS2785-1CC30-0YE0
  • In addition, the libraries for SENTRON PAC3200 and SENTRON 3VL/3WL are included in the SIMATIC powerrate Engineering and Upgrade packages. 
Libraries included (from 10/01/2009)
  WinCC PCS 7
Library SENTRON PAC3200 3ZS2791-1CC10-0YG0 3ZS2781-1CC10-0YG0
Library SENTRON 3VL/3WL Unavailable 3ZS2782-1CC10-0YG0

The following SIMATIC powerrate packages will be totally discontinued effective 10/01/2009: 

Totally discontinued SIMATIC powerrate Packages (from 10/01/2009)
  WinCC PCS 7
1 AS Runtime License  3ZS2795-1CC30-6YH0 3ZS2785-1CC30-6YH0
Unlimited Runtime License 3ZS2795-1CC30-6YD0 3ZS2785-1CC30-6YD0
Upgrade V2.0 -> V3.0
1 AS Runtime License 
3ZS2795-1CC30-6YF0 3ZS2785-1CC30-6YF0



Notes:  


- SIMATIC powerrate is currently not released for the use with the WinCC Web Navigator, WinCC Redundancy, WinCC ASIA and WinAC. 

 
- SIMATIC powerrate / WinCC:
The installation of the WinCC components AS-OS Engineering and Basic Process Control is required. For the load management and the batch-related energy consumption recording, the option package User archives is required in addition. PLCs from CPU S7-317 as well as all S7-400 can be used. 
 
- SIMATIC powerrate / PCS 7:
For the load management and the batch-related energy consumption recording, the option package User archives is required in addition.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.