×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 39026334, Entry date: 09/25/2014
(1)
Rate

GPRS/ Modbus Gateway (CE-X1)

  • Entry
  • Associated product(s)
Note The SIMATIC S7-200 components used in this application example are currently phased out. ...

Note
The SIMATIC S7-200 components used in this application example are currently phased out.
This application can be realized as easily and quickly with the new SIMATIC S7-1200.

Furthermore, many useful applications with SIMATIC S7-1200 are available here: 35923253 Task description  
Several modbus nodes, consisting of S7-200 controller and PCs, are to communicate with a modbus master in a production area of a plant. A PC-based control center is to allow visualization and logging of process values of the production area. The decentralized production area is to be analogously linked to the control center with the Micro Automation Set 21, using a GPRS network.

Solution
This Configuration Example CE-X1 helps to solve the tasks displayed. The focus is on how to understand the combination of a GPRS-system and a Modbus-System via S7-200. Furthermore how to implement it into the S7-200 PLC to work as gateway for both systems. The focus is not on the Central Station side where the Micro Automation Set 21 solution is set.

Attention
To operate a SIMATIC S7-200 with a MODEM MD720 along with the Telecontrol Server Basic, revised/new block libraries are available under the following link 99522310.

Downloads

Content of the downloads

Download

Configuration Example X1 (Documentation to the Application Example) 39026334_CE-X1_S7-200_GPRS_Modbus_DOKU_V10_e.pdf ( 386 KB )
Startup-Code for the Configuration Example X1 (STEP 7-Micro/WIN projects, WinCC flexible Visualization, SINAUT Micro SC Configuration) CE-X1_S7-200_Modbus_GPRS.zip ( 2012 KB )

Further information

Title

Link

S7-200 System manual Entry ID: 1109582
Micro Automation Set 21 Entry ID: 22537809
Modbus-library for S7-200 Entry ID: 17470979

History
First version


To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.