×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 39101287, Entry date: 10/15/2019
(4)
Rate

EDD: TH300 - HART - SITRANS DTM

  • Entry
  • Associated product(s)
Engineering Tool: SITRANS DTM Tool Version: V2.0 EDD Version: 01.01.01-04 Order number: 7NG3212-0xN00 (x=A, B, N Hardware Version: 1.0 ...
Engineering Tool: SITRANS DTM
Tool Version: V3.1
EDD Version: 01.01.04-2
Order number: 7NG3212-0xN00 (x=A, B, N
Hardware Version: 1.00
Firmware Version: >= FW 01.01.04

This is the Device Type Manager (DTM) for SITRANS TH300 HART for FDT Frame applications (e.g. PactWare) with SITRANS DTM.
For more information please check https://siemens.com/sitransTH.
New features in this update
- Support of four path measurement.
- Full support of gas features.
- enhanced support of hydrocarbon features.

SITRANS DTM - powered by EDDL
This installation file requires the software SITRANS DTM. SITRANS DTM has to be installed only once and can be downloaded from product support under the following links
SITRANS DTM 3.1 https://support.automation.siemens.com/WW/view/en/53754140
SITRANS DTM 4.1 https://support.automation.siemens.com/WW/view/en/109484287
After the installation of SITRANS DTM ,any desired device DTM can be installed. To install the device DTM ,unzip it, then double-click on the .exe file and follow the instructions. More information about the installation can be found under the following link /cs/document/61705616?caller=view&lc=en-WW

  SITRANS_TH300_HA_DTM_FDT_1_01_04_00.zip (1,6 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.