×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 39198632, Entry date: 01/08/2019
(19)
Rate

How do you do a fail-safe switch-off of standard modules?

  • Entry
  • Associated product(s)
You can do a fail-safe switch-off of various SIMATIC standard modules. This entry shows which modules apply here.

Description
In the product-related tables given below you will find SIMATIC standard modules for which you can do a fail-safe switch-off. Only the modules listed in these tables may be used for applications in which you are to do a fail-safe switch-off of SIMATIC standard modules.

The listed modules have no safety function. The safety function is triggered by the higher-level safety relay. This puts or holds the system in a safe state. You should follow the safety notes of the safety relay used accordingly.   

The following holds for a potential group in which the listed modules are located (except in the case of ET 200AL):
You may not use any additional standard digital input modules, standard analog input modules, counter modules etc. You must install a separate potential group for these.

Notes

  • Requirements for the power supply:
    For operation, you need a power supply to master overvoltages at P and M (24V). This also masters any possible common cause errors on the power supply side.
    You should select the power supply unit according to the specifications in the corresponding operating instructions for the switch-off device or system concerned.
    Detailed information about protective extra low voltages (SELV/PELV) is available in the data sheets of the power supplies to be used.
  • Plants with fail-safe features are subject to special requirements regarding operating safety on the operator's side.
    To be in a position to keep this relationship up to date or make changes to your plant you have to subscribe to the relevant newsletter. For this you log in to the Industry Online Support:
    Industry Online Support

1. ET 200SP

See also the entry entitled "Which modules can be operated in the load group of the power module F-PM-E PPM of the ET 200SP?" in Entry ID 83203124 
The following document includes corresponding wiring examples:   Wiring examples (2,2 MB) 
 

 Art. no. TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for

6ES7132-6BD20-0BA0

DQ 4x24VDC/2A STFS 03 and higherSILCL 2Cat 3/PL d
6ES7132-6BD20-0CA0DQ 4x24VDC/2A HFFS 02 and higherSILCL 2Cat 3/PL d
6ES7132-6BF00-0AA0DQ 8x24VDC/0.5A BA FS 01 and higherSILCL 2Cat 3/PL d
6ES7132-6BF00-0BA0DQ 8x24VDC/0.5A ST FS 03 and higherSILCL 2 Cat 3/PL d 
6ES7132-6BF00-0CA0DQ 8x24VDC/0.5A HF FS 02 and higherSILCL 2 Cat 3/PL d 
6ES7132-6BF01-0AA0DQ 8x24VDC/0.5A BA  FS 01 and higherSILCL 2 Cat 3/PL d 
6ES7132-6BF01-0BA0DQ 8x24VDC/0.5A ST   FS 01 and higherSILCL 2 Cat 3/PL d 

6ES7132-6BH00-0BA0

DQ
16x24VDC/0.5A ST

FS 03 and higherSILCL 2Cat 3/PL d

6ES7132-6BH01-0BA0

DQ
16x24VDC/0.5A ST

FS 01 and higherSILCL 2Cat 3/PL d 

6ES7135-6FB00-0BA1

AQ 2xU STFS 01 and higherSILCL 1 Cat 2/PL c 
6ES7135-6GB00-0BA1AQ 2xI ST FS 01 and higherSILCL 1 Cat 2/PL c 
6ES7135-6HB00-0CA1AQ 2xU/I HF FS 01 and higherSILCL 1 Cat 2/PL c 

6ES7135-6HB00-0DA1

AQ 2xU/I HSFS 01 and higherSILCL 1Cat 2/PL c

6ES7135-6HD00-0BA1

AQ 4xU/I ST

FS 03 and higherSILCL 1Cat 2/PL c


2. ET 200MP/S7-1500

The following document includes corresponding wiring examples:   Wiring examples (2,2 MB) 
 

Art. no.TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7522-1BF00-0AB0DQ 8 x DC24V 2A FS 03 and higherSILCL 2Cat 3/PL d
6ES7522-1BH01-0AB0DQ16 X DC24V 0.5A HF FS 02 and higherSILCL 2Cat 3/PL d
6ES7522-1BL01-0AB0DQ 32 X DC24V 0.5A HF FS 02 and higherSILCL 2Cat 3/PL d
6ES7522-5EH00-0AB0
DQ 16 X 24…48VUC 125VDC 0.5A ST FS 02 and higherSILCL 2Cat 3/PL d


3. ET 200eco PN

The following document includes corresponding wiring examples:  Wiring examples (2,2 MB)
 

Art. no.TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7142-6BF00-0AB08DO DC24V/1.3A FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-6BF50-0AB08DO DC24V/0.5A FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-6BG00-0AB08DO DC24V/1.3A FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-6BH00-0AB016DO DC24V/1.3A FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-6BR00-0AB08DO DC24V/2A FS 01 and higherSILCL 2Cat 3/PL d
6ES7147-6BG00-0AB08DI/DO DC24V/1.3A FS 01 and higherSILCL 2Cat 3/PL d


4. ET 200AL

The modules listed in the following table (IM, DI, DQ, DIQ, AI and IO-Link) can be used mixed in load groups in one supply line (potential group for the load power supply 2L+). You can do a fail-safe shut-off of the outputs of the output modules. The modules marked with "non-interacting" are not in fact switched off, but can be integrated in the current path of the output modules to be switched off.

The IO-Link master module is a special case. The IO-Link supply of the IO-Link devices is "non-interacting". Here you can do a fail-safe switch-off of the additional load supply. This ensures that the IO-Link communication with the IO-Link device continues if there is a switch-off.


The following document includes corresponding wiring examples:  Wiring examples (2,2 MB)

Art. no. TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7142-5AF00-0BA0

DQ 8x24VDC/2A, 8xM12

FS 01 and higherSILCL 2Cat 3/PL d

6ES7143-5BF00-0BA0

DIQ 4+DQ 4x24VDC/0.5A, 8xM8

FS 01 and higherSILCL 2Cat 3/PL d
6ES7143-5AF00-0BA0

DIQ 4+DQ 4x24VDC/0.5A, 4xM12

FS 01 and higherSILCL 2Cat 3/PL d
6ES7141-5AH00-0BA0DI 16x24VDC, 8xM12 FS 01 and higher non-interacting non-interacting
6ES7141-5BF00-0BA0DI 8x24VDC, 8xM8 FS 01 and higher non-interacting non-interacting 
6ES7141-5AF00-0BA0DI 8x24VDC, 4xM12FS 01 and highernon-interactingnon-interacting
6ES7144-5KD00-0BA0 AI 4xU/I/RTD, 4xM12 FS 02 and highernon-interactingnon-interacting
6ES7157-1AA00-0AB0 IM 157-1 DP FS 01 and higher non-interacting non-interacting 
6ES7157-1AB00-0AB0 IM 157-1 PN  FS 01 and higher non-interacting non-interacting 
6ES7147-5JD00-0BA0 

CM 4xIO-LINK, 4xM12

 FS 01 and higher

SILCL 2 non-interacting

Cat 3/PL d non-interacting


5. ET 200pro

With the ET 200pro there are still more options for switch-off. For this refer to the installation guidelines in the following FAQ response: 26694409 
>The following document includes corresponding wiring examples: Wiring examples (2,2 MB) 
 

Art. no.TypeHardware release (functional state) Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7142-4BD00-0AA04DO 24V DC/2.0A FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-4BD00-0AB04DO 24V DC/2.0A HF FS 01 and higherSILCL 2Cat 3/PL d
6ES7142-4BF00-0AA08DO 24V DC/0.5A FS 01 and higherSILCL 2Cat 3/PL d
6ES7143-4BF00-0AA04DIO/4DO 24V DC/0.5A FS 01 and higherSILCL 2Cat 3/PL d
6ES7148-4EA00-0AA016DO PNEUMATIC FS 01 and higherSILCL 2Cat 3/PL d
6ES7148-4EB00-0AA016DO PNEUMATIC FS 01 and higherSILCL 2Cat 3/PL d


6. ET 200M/S7-300

The following document includes corresponding wiring examples: Wiring examples (2,2 MB) 
 

Art. no.TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7 322-1BL00-0AA032 DO 24VDC 0.5Aab FS 10SILCL 2Cat 3/PL d


7. ET 200S

If the power supply is switched off safely, the "non-interacting" PM-Es remain active on the ET 200S backplane bus and can be used when shutting off the standard modules listed below. Furthermore, the listed standard modules can be switched off safely via PROFIsafe and PM-E F.

The following document includes corresponding wiring examples:  Wiring examples (2,2 MB)
 
Art. no.TypeHardware release (functional state)Authorized in compliance with IEC 62061 forAuthorized in compliance with ISO 13849-1 for
6ES7 132-4BB01-0AA02DO DC24V/0.5A FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BB01-0AB02DO DC24V/0.5A High Feature FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BB31-0AA02DO DC24V/2A FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BB31-0AB02DO DC24V/2A High Feature FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BD01-0AA04DO DC24V/0.5A FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BD31-0AA04DO DC24V/2A FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4BF00-0AA08DO DC24V/0.5A High Density FS 01 and higherSILCL 2Cat 3/PL d
6ES7 132-4HB01-0AB02RO NO DC24..120V/5A AC24..230V/5A FS 01 and higherSILCL 1Cat 2/PL c
6ES7 132-4HB10-0AB02 DO Relay
DC 24...48V/5A
AC 24...230V/5A
 FS 01 and higherSILCL 1Cat 2/PL c
6ES7 132-4HB12-0AB02 DO Relay
DC 24...48V/5A
AC 24...230V/5A
 FS 01 and higherSILCL 1Cat 2/PL c
6ES7 132-4HB50-0AB02RO NO/NC DC24..48V/5A AC24..230V/5A FS 01 and higherSILCL 1Cat 2/PL c
6ES7 135-4LB02-0AB02AO U High Feature FS 01 and higherSILCL 1Cat 2/PL c
6ES7 135-4MB02-0AB02AO I High Feature FS 01 and higherSILCL 1Cat 2/PL c
6ES7138-4CA01-0AA0PM-E DC24V FS 01 and highernon-interactingnon-interacting
6ES7138-4CA50-0AB0PM-E DC24..48V FS 01 and highernon-interacting non-interacting
6ES7138-4CB11-0AB0PM-E DC24..48V/AC FS 01 and highernon-interacting non-interacting
6ES7 151-1CA00-3BL0Compact device 16DI/16DO 24V/0, 5A FS 01 and higherSILCL 2Cat 3/PL d


Last Change
Complete revision with restructuring of the "Wiring examples"

Additional Keywords
Output module, Safety Integrated, Fail-safe


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.