×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 39718396, Entry date: 05/12/2020
(32)
Rate

How resistant to chemicals are the SIMATIC HMI operator panels and Industrial PCs?

  • Entry
  • Associated product(s)
Information about the chemical resistance of the fronts/surfaces of our SIMATIC HMI operator panels.

Description
The integrity of the panel front is an important criterion for ensuring the function of our panels. If environmental influences or chemical substances affect the panel front this can lead to swelling, flaking, dissolving and alteration of the panel front materials. This can also go as far as to render the panel inoperable.
To prevent this SIMATIC HMI operator panels are subjected to diverse tests, some of which are prescribed by standards. If there are no functional standards, Siemens defines what is tested and how.
The test results for SIMATIC HMI devices are given in the attached table and can be different for each panel.

  • What is tested
    Everything that is outside the control cabinet is tested. This includes device seals, housing front, front decor foil/touch foil or glass front as well as the adhesives used to hold the components together.
  • How is testing done
    From the following test conditions you can see which tests have been made on which devices. The results are given in the attached table.
    The test duration and prevailing temperature are listed in the test conditions along with the test substances. Special cases are indicated by footnotes.
  • What happens if a test substance is missing
    If a test substance is missing, it is often useful to use the results of another substance with similar chemical properties in the test conditions.
  • Customer-specific tests of other chemicals
    If a substance is not listed here, it is possible to have it tested at a charge. Get in touch with your Siemens contact about this. The costs vary depending on the time and effort, number of substances, number of test items, as well as the transport and procurement/disposal of the chemicals/test items. The costs are typically €1000 to €1500 per test, substance and temperature.

The PDF file lists all the devices whose fronts (consisting of the decor foil, plastic, seal and touch foil (on Touch devices) or glass front) have been tested and whose fronts have the same front properties as reference devices.

  39718396_device_list_e.pdf (63,9 KB) 

Note on Covid-19: How can the spread of viruses via the front panel of panels be reduced or minimized?
Here are some tips:

  • It is advisable to use protective films for submersible devices. These can also be cleaned with non-approved agents. If these then show signs of failure, they can be replaced.
  • For touch devices, a touch pen can be used as an alternative (see our touch pen system 6AV2181-8AV20-0AX0). The touch pen from the touch pen system is for both capacitive and resistive touch screens. The touch pen can also be used to operate keys on key panels. The touch pen system consists of 99.99% aluminum and can be cleaned with most disinfectants.
  • Furthermore, gloves can also be used with resistive touch systems and key devices. For capacitive touch systems (typical for glass fronts), thin latex or medical gloves may be used. However, special gloves for capacitive touch surfaces can also be used here.
    Warning: Using tools such as screwdrivers, pliers or others can lead to the destruction of the user interface or extremely limit the service life.
  • Substances that have not yet been tested can also be retested. But please note that these tests can take up to 4 months and each substance can cost approx. €1000 to €2000.
    You can request a quote for this from your Siemens contact person. Alternatively, you can also order the tests directly from TÜV or LGA. For this purpose, however, you yourself must provide the substances and the testing equipment.
  • A simple soap solution or standard detergent can also be used for damp and careful cleaning without damaging the panel fronts.

1. Chemical substances for HMI devices
The substances tested and the test conditions are listed below. The test items were coated once with the media.

Test media and test conditions
No.Test mediumTemp.
[°C]
Time
[h]
Test result
1Honing oil Castrol Honilo 9815072No recognizable change
2Super grade motor fuel2072No recognizable change
3Diesel oil2072No recognizable change
4Rape oil5072No recognizable change
5Linseed oil2072No recognizable change
6Hydrochloric acid 10%201)Test item shows signs of discoloration
7Sidolin streak-free cleaning agent with alcohol2072No recognizable change
8Caustic soda solution 10%201)Test item shows signs of discoloration
9Ethyl alcohol2072No recognizable change
10Benzine HAKU2072No recognizable change
11Solvent (alkaline)2072No recognizable change
12Acetone2072Test item shows signs of discoloration
13Brake fluid DOT 45072No recognizable change
14H²O² 10%2072No recognizable change

1) 10 cycles over a total period of 72 hours: Spray on, then leave to dry.

Remark
Adhesives do not have a long-term resistance to aggressive substances.
The fronts were exposed to the substances for a period of 72 hours. A statement about permanent exposure of the devices to substances cannot be made. The test results are based on a test period as specified in the tables.
The resistance of devices with glass front to aggressive substances is greater than that of devices with similar resistive front.

2. Single gas test in compliance with DIN EN 60068-2-42 Substances for HMI Devices
Only the fronts (consisting of the decor foil, plastic, seal and touch foil (on Touch devices) or glass front)  were tested, not the complete devices.

Test media and test conditions
No.Test gasConcentration
[ppm]
Rel. humidity
[%]
Temp.
[°C]
Time
[days]
Test result
1SO225752510No recognizable change


3. Additional chemical substances for HMI device with glass front

The substances tested and the test conditions are listed below. The evaporation of the substances was prevented by placing a PE film over the front of the test item.

Test media and test conditions
No.Test mediumTemp.
[°C]
Time
[h]
Test result
1Tap water40168No recognizable change
2Adrana D 601-01 (emulsion 20%) - Shell40168No recognizable change
3CareCut ES 3 (not water miscible) - BP40168No recognizable change
4Ecocool 0055 (emulsion 20%) - Fuchs-Dea40168 No recognizable change
5Ecocool S-HL (emulsion 20%) - Fuchs-Dea40168No recognizable change
6Ecocut 710 LE (note water miscible) - Fuchs-Dea40168No recognizable change
7Ilobroach 11 (not water miscible) - BP40168No recognizable change
8Macron 805 M- 10 VEG (not water miscible) - Shell40168No recognizable change
9Sitala A 2407 (emulsion 20%) - Shell40168 No recognizable change
10Superedge SW 133 (emulsion 20%) - BP40168 No recognizable change


4. Additional chemical substances for outdoor HMI devices

The test items were coated once with the substances. The exposure time to the substances was set to 24 hours at room temperature.


Test media and test conditions
No.Test mediumTemp.
[°C]
Time
[h]
Test result
1Methanol20>24 hNo recognizable change
2Diluting agent20>24 hNo recognizable change
3Acetic acid <50%20>24 hNo recognizable change
4Tenside20>24 hNo recognizable change
5Caustic soda solution <40%20>24 hNo recognizable change
6Aviation fuel20>24 hNo recognizable change
7Diesel oil20>24 hNo recognizable change
8Benzine20>24 hNo recognizable change
9Water20>24 hNo recognizable change
10Saltwater 5%20>24 hNo recognizable change
11H²O²20>24 hNo recognizable change
12Brake fluid20>24 hNo recognizable change


Additional Keywords
22591016, 11623359, 19137226, 6838448, Detergents, Solvents, Aggressive chemicals, Attack, Substance, Substances, Benzine, Resistance, Acid, Caustic solution, Base, Alkaline, Contaminated environment, Fluids, Robust, Sustainable, Sustainability, Resistance, Fatigue strength, Durability, Alcohol, Ethanol, Hydrogen peroxide, Propanone, Acetone, NaOH, Sodium hydroxide, Hydrochloric acid, HCl, Sulphur dioxide, Greases, Tolerance, Silicone, Clean HMI

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.