×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 39741113, Entry date: 12/08/2009
(53)
Rate

STEP 7 Basic V10.5 Service Pack 2

  • Entry
  • Associated product(s)

DESCRIPTION:

Download of Service Pack 2 for STEP 7 Basic V10.5

Installation requirements:

  • STEP 7 V10.5 (with or without SP1)

Please also read the information (What's NEW, special hints, etc.), which we have compiled for you under entry ID 40093870.

  • Customers with a valid Software Update Service agreement for STEP 7 Basic will receive the DVD with STEP 7 Basic V10.5 SP2 automatically.
  • Customers without Software Update Service agreement can download the software free of charge:
    Service Pack 2 for STEP 7 Basic V10.5 ( 679647 KB )


This free download includes the SP2 for STEP 7 V10.5 and can only be installed if the STEP 7 V10.5 software is installed already.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.