×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 39863979, Entry date: 11/13/2018
(5)
Rate

Data communication between S7-1200 stations, WinCC and TeleControl Server Basic V3.1 via CP 1242-7 V2 and CP 1243-1

  • Entry
  • Associated product(s)
An automation infrastructure contains S7-1200 substations which shall communicate cost-effectively with a central station via the mobile communications network or via Ethernet. The TeleControl Server Basic V3.1 software is installed in the central station.

The infrastructure of a discharge treatment plant comprises two S7-1200 substations. The TeleControl Server Basic V3.1 in the central station enables a direct connection to both stations. Station 1 is connected to the TeleControl Server Basic V3.1 by means of the CP 1242-7 V2 GPRS via the mobile communications network. Station 2 is directly connected to the TeleControl Server Basic V3.1 by means of the CP 1243-1 via cable-based Ethernet. WinCC Advanced, WinCC Professional and WinCC V7 can be used as OPC UA client for visualization and control of process data.

The following functions are realized in this Application Example:

  • Both remote stations send some process tags to the central station (”threshold-triggered”).
  • Both remote stations send important process tags cyclically to the central station.
  • Both remote stations send some process tags to the central station (”event-triggered”).
  • The central station monitors the status of the connected remote stations.



Advantages

  • TeleControl Server Basic V3.1 enables economic data communication between substations and the central station.
  • The data of the connected stations are available for any OPC UA client via the OPC UA interface of the TCSB.
  • GPRS and internet: Always-on functionality.
  • In case of a connection failure, the CPs buffer the data and transmit the bundled data to the TeleControl Server upon reconnection.
  • If there is a brief interruption on the connection between the OPC UA client and the TCSB OPC UA server, the data remains available in the data buffer. Once the connection has been re-established, all values that have not been transferred will be sent to the OPC UA client.

Documentation and example project with WinCC Advanced
  Documentation WinCC Advanced (3,0 MB)
 Registrierung notwendig  Project STEP 7 V15 with WinCC Advanced (2,8 MB)
 

Documentation and example project with WinCC Professional
  Documentation WinCC Professional (2,6 MB) 
 Registrierung notwendig  Project STEP 7 V15 with WinCC Professional (1,3 MB)

Documentation and example project with WinCC V7
  Documentation WinCC V7 (2,6 MB)
 Registrierung notwendig  Project STEP 7 V15 with WinCC V7 (17,2 MB)

Archive
 Registrierung notwendig  Code (STEP 7 V14) (1,2 MB)
 Registrierung notwendig  Code (STEP 7 V13 SP1) (5,1 MB)
 Registrierung notwendig  Data communication between a S7-1200 and Telecontrol Server Basic via CP 1242-7 V1 (Set30) (10,7 MB)


Further Information
Inter-Station Communication between S7-1200 Stations using TCSB V3.1 via CP 1242-7 V2
Wireless signaling and switching via SMS with S7-1200 Controllers
Teleservice of a S7-1200 with Telecontrol Server Basic

Last modification

  • Creating a Project with WinCC Professional
  • Creating a Project with WinCC V7 
  • Removal of Tag "Set 30"




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit