×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 40151404, Entry date: 01/12/2010
(0)
Rate

Release of the firmware update SINAMICS Intelligent Operator Panel (IOP) V1.0 Hotfix 1

  • Entry
  • Associated product(s)

Firmware update SINAMICS IOP (Intelligent Operator Panel)

Description

Here you will find the firmware update V1.0 Hotfix 1 for the Intelligent Operator Panel (IOP).

Overview

With the firmware update of the Intelligent Operator Panel IOP V1.0 Hotfix 1, the IOP can be additionally used with the following SINAMICS units:

  • SINAMICS G110D
  • SINAMICS CU230P-2 (with firmware release V4.3)

Installation instructions

You require a standard USB cable, type series “Series B Mini.” for the FW update
Please refer to the following document for detailed installation instructions:
 

iop-firmware-instructions-software-update-en ( 575 KB )

Download

The files to update the IOP depend on the particular hardware:

 

Please note:

After the firmware has been successfully updated, it is necessary to run the status screen wizards once in order to avoid incorrect displays!

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.