×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 40157517, Entry date: 05/11/2012
(1)
Rate

SINAMICS G/S: Speed control of a G110/S110 using S7-1200 (TIA-Portal) with USS®-Protocol (CE-X11)

  • Entry
  • Associated product(s)

Automation task
Two asynchronous motors, each of them connected to the SINAMICS G110 frequency inverter, are to be controlled by an S7-1200 controller (CPU1211C) via the CM1241 (RS485) communication module. Communication between controller and frequency inverter takes place with the aid of the USS protocol. A KTP600 touch panel that is connected to the S7-1200 controller via an Ethernet connection is used for operation and visualization. STEP 7 Basic V10.5 is used as a configuration tool for the control program and the HMI.

The motors are to be operated on speed. A setpoint from 0 to 100% is specified. It is to be possible to change the direction of rotation and to acknowledge drive errors. During runtime it is to be possible to read and change parameters of the frequency inverter via the USS protocol. The actual speed is to be displayed together with the drive status.


Figure 01

Startup Code
For the startup we offer you software examples with test code and test parameters as download. These software examples support you in the first steps and tests of the configuration examples. They enable a quick test of hardware and software interfaces of the products described in the configuration example.

Downloads

Content of the downloads

Download

Configuration Example documentation ConfigurationExample_x11_S7-1200_G110_v1d1_en.pdf ( 1706 KB )
Startup Code V1.0 with control program for CPU 1211C and HMI project for KTP600 (STEP 7 Basic V10.5) CE_x11_S7-1200_v1d0.zip ( 10294 KB )
Project Example V1.0 for SINAMICS S110 (STARTER v4.1 SP5 HF1) CE_x11_STARTER_S110_v1d0.zip ( 731 KB )

Links

Contents of the links

Link

S7-1200 System manual 36932465
Description USS Protokoll 24178253
Configuration Example X9 - Distributed positioning with S7-1200 and SINAMICS S110 40616058
Low Voltage Inverters for General Applications SINAMICS Link
SINAMICS S110 Link
In TIA Portal V11, how do you update the library blocks after converting a STEP 7 V10.5 project? 59421832

History

Version

Modifications

December 2009 First edition
January 2010 Addition Project Example STARTER
April 2012 Addition link to entry ID how to update the USS library blocks after converting the STEP 7 Basic V10.5 project to STEP 7 V11

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.