Entry type: FAQ Entry ID: 40227286, Entry date: 10/30/2019
(18)
Rate

What are the functional differences between the different SIMATIC panels?

  • Entry
  • Associated product(s)
This FAQ response shows you different ways of obtaining a comparison of the technical data of the SIMATIC HMI operator panels.

TIA Selection Tool

The TIA Selection Tool provides you with convenient comparison options for selecting an operating device according to your technical demands.
Home page of the TIA Selection Tool


Siemens Industry Mall

The Siemens Industry Mall includes a comprehensive catalog of all the available components along with their technical data. Enter the article number of a specific panel or its type designation to obtain all the product information.
Home page of the Siemens Industry Mall


WinCC (TIA Portal) Manuals and ST 80 Catalog

Detailed technical information on the SIMATIC HMI operator panels is available in the documents below.

  • In the manuals for
    SIMATIC STEP 7 Basic/Professional V15 and SIMATIC WinCC V15
    (Entry ID: 109755202, Chapter 13 "Visualizing processes" > 16 "Performace features").
  • In the ST 80 Catalog 109744146
  • In the manuals of the panels concerned.


Siemens Industry Online Support

In the Siemens Industry Online Support, in the Find mask on the right, you enter the type designation or the article number of the device concerned and then select the desired model under "Product Links".
In the overview that opens you select the link "Technical Data".


WinCC flexible and WinCC (TIA Portal) Online Help

Further information about the scope of functions of the SIMATIC HMI operator panels is available in the Online Help of WinCC flexible and WinCC (TIA Portal).


Operator panels for hazardous areas with potentially explosive atmosphere

An overview of which operator panels you can use in hazardous areas with potentially explosive atmosphere is available in Entry ID: 291285.

Additional Keywords
Basic Panel, Basic Panel 2nd Generation, Mobile Panel, Multi Panel, Comfort Panel, Panel comparison, Panel functions, Panel function comparison, Smart devices, WinCC, Windows Mobile, Operating system, OS, Pictures, Tags, Analog messages, Bit messages, Recipes, Tag archives, Message archives, Audit, Audit Trail, Scripts, Logs, Text list, Graphics list, User administration, Faceplates, ProAgent, WinAC MP, Buttons, Graphics display, IO field, Switches, Bar display, Performance features, Function features, Operator panel overview, System limits, Slider, Smart, Sm@rt, Server, Sm@rt server, Sm@rt client, HTML browser, User display, Internet Explorer, Pointer instrument, Trend display, Symbol library, Recipe display, Alarm display, Message window, Alarm indicator, flexible, WinCC flexible, Function, Functions, Elements, Comparison, CPU, Diagram, Properties, Technical data, Basic, Comfort, TIA Portal, Diagnosis display, Safety, Number of connections, 15363798

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.