×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 40545919, Entry date: 01/06/2010
(0)
Rate

How do I order a SITRANS FX300 Vortex flowmeter?

  • Entry
  • Associated product(s)

QUESTION:  

How do I order a SITRANS FX300 Vortex flowmeter?

ANSWER:  

In order to enable the application specific data processing, SITRANS FX300 is programmed from factory with data entered by you during ordering. This makes ordering a Vortex flowmeter different from other ordering processes.

The SITRANS F X meter is ordered as follows:

  1. Start up the order by choosing the right size of meter by using the sizing tool.
    (Go to https://pia-portal.automation.siemens.com/default.htm; select language; select the “Sizing” tab; click on “Start -> Flow -> SITRANS F X sizing” and install the program).

  2. Enter the PIA-Selector and configure the right MLFB code

  3. Carefully enter the Y option fields by filling in the input process data including the units.

Y40-Y45 has to be filled out in order to start up an order:

Field

Input data

Example

Y40

Specify the medium: steam, gas or liquid

Steam (superheated)

Y41

Specify the max operating temperature, limit is: -40…+240°C [-40…+464°F]

220°C

Y42

Specify the max operating pressure, limit of media pressure is max. 100 bar

10 Bar g

Y43

Specify the density (if non std. / unknown medium)

5,10469 kg/m³

Y44

Specify the Viscosity (if non std. / unknown medium)

0,0167287 mPa.s

Y45

Specify the max flow-rate.
Run the calculation, select the suitable selections (green) and check the sizing results if the selection matches your min. flow range as well

Max. Flowrate = 500 kg/h

See an example of filled out Y option fields in attached image.

Title of the Download
 Yoptions.jpg ( 64 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.