×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 40616248, Entry date: 07/25/2014
(3)
Rate

Wireless Signalling and Switching per SMS with S7-1200 controller (Set 25)

  • Entry
  • Associated product(s)
Description   A GSM modem SINAUT MD720-3 is to be linked with a SIMATIC S7-1200 controller. With the aid of the modem messages (SMS) can be sent to mobilephones or other Remote Stations. Receiving SMS is also possible. ...

Description  
A GSM modem SINAUT MD720-3 is to be linked with a SIMATIC S7-1200 controller. With the aid of the modem messages (SMS) can be sent to mobilephones or other Remote Stations. Receiving SMS is also possible.


Fig. 01

In order to better illustrate the necessary functions and features of this application, a rainwater retention basin is assumed as example. Measures for efficient maintenance should be taken for optimizing plant availability and efficiency. Alarm messages for instance in case of malfunction of the lock should be sent to the service personnel as an SMS message via this GSM modem. Following use cases are considered.

Solution  
This configuration example CE-X25 helps to solve the tasks displayed. The focus is on the library blocks which enable SMS-Sending and SMS-Receiving.


Fig. 02

Downloads

Content of the downloads

Download

Library description on the Configuration Example X25 (Documentation for the implemented STEP 7 V11 library) 40616248_LibraryDescription_S7-1200_SMS_DOKU_V12_e.pdf ( 726 KB )
Library for STEP 7 Basic V11
Containing also the outdated library based on STEP 7 V10.5 
CE-X25_S7-1200_SMS_library.zip ( 1141 KB )
Configuration Example X25 (Documentation based on the Startup-Code) 40616248_ConfigurationExample_S7-1200_SMS_DOKU_V12_e.pdf ( 870 KB )
Startup-Code (Project file for STEP 7 V11)
Containing also the outdated project file based on STEP 7 V10.5
CE-X25_StartupProject.zip ( 5007 KB )

Further information

Titlee

Link

Wireless signaling and switching via SMS with S7-1200 Controllers an CP1242-7 (Set 32) Entry ID: 58638283
S7-1200 System manual Entry ID: 36932465
S7-200 based remote communication solution with SMS Entry ID: 21063345
S7-300 based remote communication solution with SMS Entry ID: 25545680
Conference in the technical Forum of the Service & Support Portal concerning Applications link


To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Last change
Figures, Security Notice

Additional Keywords
wireless, m2m, without server


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.