×
Siemens Industry Online Support
Siemens AG
SiePortal
Entry type: Product note Entry ID: 40839811, Entry date: 01/28/2010
(0)
Rate

Possible malfunction of SCALANCE W786

  • Entry
  • Associated product(s)
SCALANCE W786 - order numbers: 6GK5786-1AA60-2AA0, 6GK5786-1BA60-2AA0, 6GK5786-2AA60-2AA0 and 6GK5786-2AA60-1CA0 - product version 4 and 5 (copper versions), date of manufacture January 2009 to August 2009, can fail to start at cold restart.

  In the case of the SCALANCE W786 from the period of manufacture given above, the devices may fail to start up after a cold restart (e.g. following power failure, reconfiguration, or new configuration). The fault does not occur during operation.

You can download the file with the affected serial numbers Here ( 109 KB ) .

Determining the serial number on the device:

 

 

Please consult your contact at your local Siemens branch to discuss replacement or repair of the SCALANCE W786.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.