×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 40845590, Entry date: 06/10/2010
(0)
Rate

SIRIUS Innovations Compact Starter with IO-Link Connection to the Control and Integration into STEP 7(CE-FE-III-010-V20-EN)

  • Entry
  • Associated product(s)

The aim of the Appllikation
The use of compact starters with IO-Link facilitates use in decentralized solutions. This ensures connection to the TIA environment. This application shows the structure of compact starters using conveyors in a conveyor system and their integration into STEP 7.

Solution
For the control of band conveyors positioned close to one another within the system, the compact starters can be constructed in a control cabinet. Connection to the control is implemented via IO-Link.

 

Downloads

Content of Downloads

Download

Documentation (German)  CE-FE-III-010-V20-DE.pdf ( 560 KB )
Documentation (English)  CE-FE-III-010-V20-EN.pdf ( 525 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.