×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 41140750, Entry date: 06/02/2010
(0)
Rate

SIRIUS Innovations Load Feeder with IO-Link Connection to the Control and Integration into STEP 7(CE-FE-III-012-V20-EN)

  • Entry
  • Associated product(s)

The aim of the Appllikation
For the control of conveyors positioned at a distance from one another within the system, the load feeders are supplied via a power bus. The diagram below shows an example of a conveyor with a turntable. Connection to the control is implemented via the IO-Link master.

Solution
In small or locally concentrated systems, the drives can be controlled in a control cabinet.

 

Downloads

Content of Downloads

Download

Documentation (German)  CE-FE-III-012-V20-DE.pdf ( 549 KB )
Documentation (English)  CE-FE-III-012-V20-EN.pdf ( 534 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.