×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 41141976, Entry date: 06/01/2010
(1)
Rate

SIRIUS Innovations Load Feeder with AS-Interface Connection to the Control and Integration into STEP 7(CE-FE-III-011-V20-EN)

  • Entry
  • Associated product(s)

The aim of the Appllikation
The use of function modules with AS-Interface facilitates use in decentralized solutions. This ensures connection to the TIA environment. This application shows the structure of load feeders using conveyors in a conveyor system and their integration into STEP 7.

Solution
For the control of conveyors positioned at a distance from one another within the system, the load feeders are supplied via a power bus. The diagram shows an example of a conveyor with a turntable. Connection to the control is implemented via AS-Interface.

 

Downloads

Content of Downloads

Download

Documentation (German)  CE-FE-III-011-V20-DE.pdf ( 323 KB )
Documentation (English)  CE-FE-III-011-V20-EN.pdf ( 297 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.