×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 41142014, Entry date: 02/09/2010
(0)
Rate

Delivery Release of the SIPLUS S7-1200 Product Range for Extreme Environmental Conditions

  • Entry
  • Associated product(s)

Refined products for extreme environmental conditions from the SIPLUS S7-1200 range are available as of now. All versions offer protection with extended temperature ranges and against medial loads, e.g. aggressive industrial atmospheres.

Date for the Release for Delivery : 2010-01-06



Product description:
The refined SIPLUS products are based on the respective basic types 6ES72*, 6EP* for normal application areas. Therefore, the general technical data are applicable in addition to the special features for extended temperature range, condensation, increased humidity or extraordinary medial loads, e.g. corrosive gas atmospheres.

Refined products for extreme environmental conditions from the SIPLUS S7-1200 range are available as of now. All versions offer protection with extended temperature ranges and against medial loads, e.g. industrial atmospheres such as corrosive gases, humidity, salts, etc.  Furthermore, they are suitable for condensation. Even though application is supported in the ambient temperature range from -25 to +70 °C, the following exception has to be observed:
SB modules cannot be employed in this extended temperature range as their installation bay on the SIPLUS CPU module is occupied by a heat sink. Furthermore, only 50% of IOs per module must be controlled simultaneously at temperatures from +60 °C. CPU versions which are applicable without restrictions are available for the temperature range from -25 to +55 °C .
This way, all required functions are supported as an optimum solution from the SIPLUS S7 portfolio is available for all customer requirements.

For further information, please refer to:http://www.siemens.com/siplus 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit