×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4124504, Entry date: 08/27/1996
(0)
Rate

Ability of COM Software to Execute Under STEP5/ST V6.6, Part 2

  • Entry
  • Associated product(s)
                                                                            

                                                                            

                                                                            

_Earlier test results:_                                                     

                                                                            

The results of the tests of COM packages published in SIMATIC S5            

Infos  94/01/016 and /017 as well as 95/14/022 to /024 are still            

valid if they are not superseded by the information below.                  

                                                                            

_General:_                                                                  

                                                                            

If you should experience problems with a COM package or optional            

package in the DOS window, we recommend to operate STEP 5/ST in             

full-screen mode or directly under MS-DOS 7.0.                              

                                                                            

In general, we also recommend to operate STEP 5/ST in the full-             

screen mode of Windows '95.                                                 

                                                                            

                                                                            

_Legend for the table below:_                                               

                                                                            

ok        : COM package has been successfully tested.                       

(ok)      : COM package will execute with limitations.                      

kF        : Not released for STEP 5, version 6.6.                           

--        : Not tested.                                                     

DOS-BOX   : Test was carried out in a DOS-Box under Windows '95.            

FullScreen: Test was carried out in a DOS-Box under Windows '95             

            in full-screen mode (no change of tasks).                       

DOS 7.0   : Test was carried out under DOS 7.0.                             

                                                                            

                                                                            

----------------------------------------------------------------            

Package  Version  Catalog No.             Result                            

----------------------------------------------------------------            

NCM COM                                                                     

5430 TF     (A2)  6GK1 745-1AC00-0EA0     DOS-BOX     --                    

                                          FullScreen  --                    

                                          DOS 7.0     ok                    

Pecularities: None                                                          

-----------------------------------------------------------------           

NCM COM                                                                     

5431 FMS    (A1)  6GK1 745-1AD0.-0EA0     DOS-BOX     --                    

                                          FullScreen  --                    

                                          DOS 7.0     ok                    

Peculiarities: None                                                         

-----------------------------------------------------------------           

PRO 100     V1.0  6ES5 805-0PA12          DOS-BOX     --                    

                                          FullScreen  --                    

                                          DOS 7.0     ok                    

Peculiarities: In the CONFIG.SYS, the driver ANSI.SYS                       

              must be loaded.                                               

-----------------------------------------------------------------           

                                                                            

                                                                            

                                                                            

-----------------------------------------------------------------           

PMCPRO WIN  V2.3  6ES5 886-4WF.1          DOS-BOX     --                    

                                          FullScreen  --                    

                                          DOS 7.0     --                    

Peculiarities: Windows application; will execute under                      

              Windows '95 only.                                             

-----------------------------------------------------------------           

ProFuzzy    A01   6ES5 834-3MG.1          DOS-BOX     ok                    

                                          FullScreen  --                    

                                          DOS 7.0     --                    

Peculiarities: None                                                         

-----------------------------------------------------------------           

SIEPIDS5    V2.1  6ES5 834-3MA.1          DOS-BOX     ok                    

                                          FullScreen  --                    

                                          DOS 7.0     --                    

Peculiarities: None                                                         

-----------------------------------------------------------------           

SIFLOCS5    V2.1  6ES5 834-3MF.2          DOS-BOX     ok                    

                                          FullScreen  --                    

                                          DOS 7.0     --                    

Peculiarities: None                                                         

-----------------------------------------------------------------           

TK 858                                    DOS-BOX     ok                    

                                          FullScreen  ok                    

                                          DOS 7.0     ok                    

Peculiarities: None                                                         

-----------------------------------------------------------------           

TS 758 S    V3.2                          DOS-BOX    (ok)                   

                                          FullScreen (ok)                   

                                          DOS 7.0     ok                    

Peculiarities:Depending on the configuration of the target device           

            it may be necessary to start Teleservice in DOS mode.           

-----------------------------------------------------------------           





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.