×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4129320, Entry date: 08/27/1996
(0)
Rate

S5-95U with L2-DP Slave Interface - New Revision Level 02

  • Entry
  • Associated product(s)
                                                                            

                                                                            

Concerns the product with Catalog No.:                                      

                                                                            

6ES5 095-8MD01   S5-95U mini PLC with L2-DP slave interface                 

                                                                            

                                                                            

                                                                            

_Reason for the change:_                                                    

                                                                            

The new revision level includes the following additional func-              

tions:                                                                      

                                                                            

- As published in SIMATIC Info 95/02/17, the user memory has been           

  expanded from 16 to 20 Kbytes, of which 16 Kbytes are for user            

  programs (OB, FB, PB, SB) and data, and 4 Kbytes are for data             

  only.                                                                     

                                                                            

- The watchdog timer of the AS 511 interface can now be set in              

  system data SD56. The value entered in SD56 is multiplied by              

  10ms. If an overall reset is made, a default value of 50                  

  (= 500ms) is used.                                                        

  Permissible range: 2 to 255 (20 ms to 2550 ms).                           

                                                                            

- Adaptations have also been made to account for the changes                

  in the PROFIBUS DP, DIN E 19245, Part 3, standard.                        

                                                                            

Please speak to your SIMATIC contact at your local Siemens                  

office about an upgrade.                                                    

                                                                            

                                                                            

                 -------------------------------                            





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.