×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 41307046, Entry date: 06/16/2016
(11)
Rate

SIMATIC Temperature Control TCP 3000

  • Entry
  • Associated product(s)
TCP 3000 is used to control temperature zones in the plastics sector. This includes, for example, extruder heating zones or tool heating zones.

Besides the self-optimized adjusting core, various additional functions round off the fields of use of the controller.

Note
If you are interested, please contact your local sales partner.
Contacts worldwide   

Download
  E-Flyer TCP-3000 en (2013; 225,7 KB) 

Update (2016-05-04)
As part of our continuous product improvement, we have noticed a deviation in the temperature control application TCP3000.
For deliveries since 10/2009, it may happen once, that in the worst case, when putting the time forward, the controller and outputs are not updated (refreshed) for 32 seconds (usually less).
For all new applications this behavior was removed as of 05/2016, V01.06.03.
For older systems, retrieve the update in the SIMATIC Manager and then follow the instructions in the SCL source "HowToImplement_EN.SCL" 
 Registrierung notwendig  41307046_Update_2016_05_04_OB1.zip (286,4 KB) 

Search terms
Temperaturregler, Extrusion, temperature controller, SIMATIC S7, motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.