×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4138588, Entry date: 08/27/1996
(0)
Rate

Installing the COM ET 200 V3.1 Software on a PG 685 Programmer

  • Entry
  • Associated product(s)
                                                                            

_- Product Information                                         _            

                                                                            

Concerns the product with Order No.:                                        

                                                                            

6ES5 895-6SE.1   COM ET 200 with Manual                                     

                                                                            

                                                                            

                                                                            

It is possible to install the COM ET 200, V3.1 software on a                

PG 685 programer under S5-DOS/ST (PCP/M), provided the following            

prerequisites are fulfilled:                                                

                                                                            

- S5-DOS/ST (PCP/M), stage V, version 3.2 operating system,                 

- At least 1 Mbyte of free capacity on the hard disk.                       

                                                                            

After transferring the COM ET 200 files to the hard disk with               

the command:                                                                

                                                                            

- pip b:=a:*.*Äg0rvw                                                        

                                                                            

the file S5WX003H.CMD must be copied into the file S5WX005H.CMD             

on the hard disk. Command:                                                  

                                                                            

- pip S5WX005H.CMD=S5WX003H.CMDÄrvw                                         

                                                                            

This data transfer is necessary if the COM ET 200 software is to            

execute on a PG 685 programmer.                                             

                                                                            

"On-line functions" with the COM ET 200 and the PG 685 are not              

possible and may not be selected.                                           

                                                                            

                                                                            

                 -------------------------------                            





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.