Entry type: FAQ, Entry ID: 415725, Entry date: 04/24/2015
(0)
Rate

How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?

  • Entry
  • Associated product(s)
This entry provides you with information about the connection resources of the S7-300 and S7-400 CPUs.

The maximum number of connections and communication jobs that an S7-300 or S7-400 supports depends on the CPU and CP used.
Each connection requires connection resources for the end point or for the transition point (CP, for example) on the stations concerned. The number of connection resources is CPU/CP-specific. If all the connection resources of a communication partner are occupied, no new connection can be set up.

TheTechnical Data of the S7-300 CPUsprovides with information about the maximum number of connection resources.

TheTechnical Data of the S7-400 CPUs provides you with information about the maximum number of connection resources.

Information about the maximum permitted number of simultaneous connections via CP is available in the relevant CP manuals in the chapter entitled "Performance Data".

An overview of the services and quantity frameworks that the CPUs with integrated PN interface support is available in Entry ID: 18909487.

An overview of the services and quantity frameworks that the Industrial Ethernet CPs of S7-300 and S7-400 support is available in Entry IDs: 16767769 and 15368142.

Information about how the communication resources are assigned in the S7-300 is available in Entry ID: 97649464.

Information about which communication connections of the Industrial Ethernet CPs need connection resources of the CPU is available in Entry IDs: 42480411 and 42480718.

 

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster