×
Siemens Industry Online Support
Siemens AG
SiePortal
Entry type: Product note Entry ID: 4169975, Entry date: 08/27/1996
(0)
Rate

ET100U/IM 308 Interface Module - Error in the Product Manual

  • Entry
  • Associated product(s)
                                                                            

                                                                            

Concerns products with the Order Nos.:                                      

                                                                            

6ES5 308-3UA12   ET 100U, IM 308 Interface Module                           

6ES5 998-2DP.1   Product Manual for Distributed I/Os                        

                                                                            

                                                                            

The Product Manual "Distributed I/Os, Interface Modules 308-3U/             

318-3U" (Order No. 6ES5 998-2DP*1) contains an error on page                

2-2. Some restrictions exist regarding the use of multiple                  

IM 308 modules in one PLC or EU of the S5-150U or S5-155U.                  

                                                                            

The IM 308-3UA12 can be plugged into the following module loca-             

tions:                                                                      

                                                                            

S5-155U: No restrictions:    Locations 155, 163                             

         With restrictions:  Locations 139, 147 (no CP may be               

                             plugged into locations 139 or 147 at           

                             the same time)                                 

                                                                            

S5-150U: No restrictions:    Location 139, 147, 155, 163                    

         With restrictions:  Locations 107, 115, 123, 131 (no CP            

                             may be plugged into these locations            

                             at the same time)                              

                                                                            

S5-135U: No restrictions:    Locations 139, 147, 155, 163                   

                                                                            

S5-115U                                                                     

  CR 700-2: No restrictions: Location 6                                     

  CR 700-3: No restrictions: Location 6                                     

                                                                            

EU 185U: No restrictions:    Location 147, 155, 163                         

                                                                            

EU 186U: No restrictions:    Location 131, 147, 163                         

                                                                            

Please correct your Manual accordingly.                                     

                                                                            

                                                                            

                 -------------------------------                            





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.