×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 41726666, Entry date: 04/15/2010
(1)
Rate

How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?

  • Entry
  • Associated product(s)

Description
The documentation included in this entry describes how to connect a SIMATIC MV440 code reading system to a SIMATIC S7-300 via PROFINET IO.
In this example, a CPU319-3PN/DP is used as PROFINET IO controller.

The following figure illustrates this device configuration.


Fig. 01

Documentation
PROFINET_IO_with_MV440_en.pdf ( 1857 KB )

Sample programs
The "41726666_PROFINET_IO_with_MV440.zip" file provides the following sample programs and the components required as a download.

  • The STEP 7 project "MV440.zip" that includes the configuration of a CPU319-3PN/DP as PROFINET IO controller and a SIMATIC MV440 code reading system as PROFINET IO device. The sample program "Example.zip" is integrated in the STEP 7 application program of the CPU319-3PN/DP.
  • The sample program "Example.zip" that is on the CD included in the delivery package of the SIMATIC MV440 code reading system.
  • The GSD file of the SIMATIC MV440 code reading system, which is on the CD included in the delivery package of the SIMATIC MV440 code reading system.

PROFINE_IO_with_MV440.zip ( 841 KB )

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.