×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 41931553, Entry date: 03/18/2010
(0)
Rate

How Is The SITRANS FX300 Current Output 4-20ma Set Up?

  • Entry
  • Associated product(s)

QUESTION:  

How Is The SITRANS FX300 Current Output 4-20ma Set Up?

ANSWER:  

The Current Output setting is as follows:

• 20mA represents the Qmax setting
• 4mA represents no flow or zero flow
• The current output by Qmin can be calculated using the sizing program

Link to sizing program:
https://pia-selector.automation.siemens.com/sap/its/mimes/zstore3/40/xx/sizing_tools/vortexsizing.zip


Values below the Qmin setting will not be registered in the totalizer – the value will be
displayed as zero.


Download printerfreindly version (pdf)
How Is The SITRANS FX300 Current Output 4-20ma Set Up? ( 62 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.