×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4202341, Entry date: 02/25/1997
(0)
Rate

Digital Output Modules 451-4UA14 and 454-4UA14 - New Revision Level 2

  • Entry
  • Associated product(s)
                                                                            

                                                                            

Concerns products with the catalog Nos.:                                    

                                                                            

6ES5 451-4UA14    451 dig. outp. module for S5-135/155U                     

6ES5 454-4UA14    454 dig. outp. module for S5-135/155U                     

                                                                            

_Reason for the change:_                                                    

                                                                            

In the case of unfavourable voltage fluctuations of the 24 V load           

voltage, the short-circuit indication of the 6ES5 451-4UA14 and             

6ES5 454-4UA14 digital output modules may be wrong. The red short-          

circuit LED will light up briefly, although there is no short circuit.      

                                                                            

In isolated cases there will even be a permanent short-circuit              

LED signal as well as a short-circuit output signal at the front            

connector of the module.                                                    

                                                                            

Nevertheless, proper functioning of the module and of the short-            

circuit protection are assured.                                             

                                                                            

_Upgrading_                                                                 

                                                                            

The above problem has been eliminated with revision level 2 of the          

modules. If the fault occurs with one of your modules, please speak         

to your SIMATIC contact at your Siemens office about an upgrade.            

                                                                            

                                                                            

                  ------------------------------                            





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.