×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 42200753, Entry date: 04/08/2010
(0)
Rate

Model Predictive Control including integral transfer functions

  • Entry
  • Associated product(s)
Objective of the application is the dimensioning of the model predictive controller provided in SIMATIC PCS 7 if the process is not stable or shows an integral action (e.g. level control, position control).

Objective of the Application
The area of application of the model predictive controller provided in SIMATIC PCS 7 (function block ModPreCon and MPC respectively) is restricted by the following fact: The control algorithm only works for stable processes with a step response settling to a constant value in a finite time horizon.
If the process is not stable or shows an integral action (e.g. level control, position control), the respective sub transfer functions have to be stabilized by slave con-trollers. The objective of this application note is to describe how to proceed in such cases.
This application note is an extension of the application note "Multivariable Model Predictive Control – the Distillation Column as an Application Example", containing basic information how to apply the MPC.
The application example considered here shows an MPC with two manipulated and two controlled variables in combination with a simulated process of which the sec-ond main control loop shows integral action.

Main contents
The following main points are discussed in this application note:

  • The stabilization of unstable processes using P(ID) controllers
  • The integration of a subordinated PID controller in an MPC application
  • Simulation example

Validity
This entry was created with SIMATIC PCS 7 V7.0 SP1, the procedure is transferable to higher PCS 7 versions.

Downloads
  Model Predictive Control including integral transfer functions (12,0 MB) 

History
04/2010 First release


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit