×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 42492834, Entry date: 06/01/2010
(0)
Rate

Extended Range of Packages for SIMATIC Industry PCs and SIMATIC S7-mEC

  • Entry
  • Associated product(s)

The range of packages for the SIMTIC Industry PC has been extended by packages with SIMATIC WinAC RTX / WinAC RTX F software controllers, and for the SIMATIC S7-mEC by HMI packages with WinCC flexible.
As before, the Industry PC / S7-mEC and the software package must be ordered with one order.

Our offer of software packages has been extended by packages with SIMATIC WinAC RTX and WinAC RTX F software controllers for all SIMATIC Industry PCs. Packages with SIMATIC WinCC flexible can now also be ordered together with the SIMATIC S7-mEC embedded controller.

Packages with WinCC flexible, WinAC RTX and WinAC RTX F
The list of released SIMATIC Industry PCs has been expanded by the embedded IPC 427C and 477C and now includes:

  • Panel PC 577B and 677 / 677B
  • HMI IPC477C and 577C
  • IPC427C
  • Box PC 627B and 827B
  • Rack PC 547B / 647B and 847B
  • IPC547C

The embedded IPCs 427C and 477C are also available as bundle with preinstalled software.


Packages with WinCC flexible
The SIMATC S7-mEC with order no. 6ES7 677-1* has been released.
As is the case with the SIMATIC Industry PCs, bundles with preinstalled software are also available for the S7-mEC.

Packages with WinCC
The list of released SIMATIC Industry PCs has been expanded by the embedded IPCs 427C and 477C and now includes:  

  • Panel PC 577B and 677 / 677B
  • HMI IPC577C
  • Box PC 627B and 827B
  • Rack PC 547B / 647B and 847B
  • IPC547C
  • HMI IPC477C and IPC427C (only released together with Windows XP professional)

The embedded HMI IPC477C is also available as bundle with preinstalled software.
 

Order no.'s for packages with SIMATIC software:

SIMATIC WinAC (always latest version)

Package: WinAC RTX  2009 6ES7 671-0RC07-6YA0
Package: WinAC RTX F 2009 6ES7 671-1RC07-6YA0

SIMATIC WinCC flexible (always latest version)

Package: WinCC flexible  2008; RT 128 Power Tags 6AV6623-2BA00-0AA0
Package: WinCC flexible  2008; RT 512 Power Tags 6AV6623-2DA00-0AA0
Package: WinCC flexible  2008; RT 2048 Power Tags 6AV6623-2FA00-0AA0
Package: WinCC flexible  2008; RT 4096 Power Tags 6AV6623-2GA00-0AA0

SIMATIC WinCC V7.0 SP1

WinCC Package V7.0, RT 128 Power Tags 6AV6382-2CA07-0AX0
WinCC Package V7.0, RT 512 Power Tags 6AV6382-2DA07-0AX0
WinCC Package V7.0, RT 2048 Power Tags 6AV6382-2EA07-0AX0
WinCC Package V7.0, RT 8192 Power Tags 6AV6382-2HA07-0AX0
WinCC Package V7.0, RT 65536 Power Tags 6AV6382-2FA07-0AX0

SIMATIC WinCC V6.2 SP3

WinCC Package V6.2, RT 128 Power Tags 6AV6382-2CA06-2AX0
WinCC Package V6.2, RT 256 Power Tags 6AV6382-2DA06-2AX0
WinCC Package V6.2, RT 1024 Power Tags 6AV6382-2EA06-2AX0
WinCC Package V6.2, RT 8192 Power Tags 6AV6382-2HA06-2AX0
WinCC Package V6.2, RT 65536 Power Tags 6AV6382-2FA06-2AX0

Important:
One of the listed SIMATIC software packages (Runtime) must be ordered together with the one of the listed Indutry PCs.
Subsequent package orders will not be accepted anymore.
When you select the hardware please note the minimum requirements / preconditions of the software with respect to the hardware.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.